<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx25 internal RAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222167#M14817</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to load and execute a program in the imx25 internal RAM, either via the serial downloader or from SPI flash.&amp;nbsp; Is this possible?&lt;/P&gt;&lt;P&gt;I am assuming some portions of internal RAM are used by the ROM code and would be off limits.&amp;nbsp; I don't find much information on internal RAM in the imx25 reference manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2013 19:18:57 GMT</pubDate>
    <dc:creator>rbruce</dc:creator>
    <dc:date>2013-01-09T19:18:57Z</dc:date>
    <item>
      <title>imx25 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222167#M14817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to load and execute a program in the imx25 internal RAM, either via the serial downloader or from SPI flash.&amp;nbsp; Is this possible?&lt;/P&gt;&lt;P&gt;I am assuming some portions of internal RAM are used by the ROM code and would be off limits.&amp;nbsp; I don't find much information on internal RAM in the imx25 reference manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 19:18:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222167#M14817</guid>
      <dc:creator>rbruce</dc:creator>
      <dc:date>2013-01-09T19:18:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx25 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222168#M14818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hope the enclosed example helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 11:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222168#M14818</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-01-10T11:11:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx25 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222169#M14819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the example.  After a quick look at the files, I think this will help me accomplish what I want to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert W.(Bill) Bruce&lt;/P&gt;&lt;P&gt;Watlow&lt;/P&gt;&lt;P&gt;Winona, MN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 14:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222169#M14819</guid>
      <dc:creator>rbruce</dc:creator>
      <dc:date>2013-01-10T14:57:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx25 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222170#M14820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK.  I’m running a small program from internal RAM based on the sample you sent .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks very much for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert W. (Bill) Bruce&lt;/P&gt;&lt;P&gt;Watlow&lt;/P&gt;&lt;P&gt;Winona, MN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 20:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx25-internal-RAM/m-p/222170#M14820</guid>
      <dc:creator>rbruce</dc:creator>
      <dc:date>2013-01-10T20:25:32Z</dc:date>
    </item>
  </channel>
</rss>