<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックArmhf linux for iMX6ul evk</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Armhf-linux-for-iMX6ul-evk/m-p/996387#M147825</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon. I need to make armhf linux for iMX6ul. When I bitbake image-core-base, then "uname -a" command return that system has armel architecture and noway to install armhf package with apt-get. How can I configure bitbake to create the armhf linux with frame-buffer, but without x-server or wayland.&lt;/P&gt;&lt;P&gt;I thought that iMX6ul is armhf CPU...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Nov 2019 11:46:32 GMT</pubDate>
    <dc:creator>ATAineri</dc:creator>
    <dc:date>2019-11-15T11:46:32Z</dc:date>
    <item>
      <title>Armhf linux for iMX6ul evk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Armhf-linux-for-iMX6ul-evk/m-p/996387#M147825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon. I need to make armhf linux for iMX6ul. When I bitbake image-core-base, then "uname -a" command return that system has armel architecture and noway to install armhf package with apt-get. How can I configure bitbake to create the armhf linux with frame-buffer, but without x-server or wayland.&lt;/P&gt;&lt;P&gt;I thought that iMX6ul is armhf CPU...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2019 11:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Armhf-linux-for-iMX6ul-evk/m-p/996387#M147825</guid>
      <dc:creator>ATAineri</dc:creator>
      <dc:date>2019-11-15T11:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: Armhf linux for iMX6ul evk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Armhf-linux-for-iMX6ul-evk/m-p/996388#M147826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vladislav Redin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Armhf is a Debian port, you can find more information below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.debian.org/ports/#portlist-released"&gt;https://www.debian.org/ports/#portlist-released&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BSP release is not based on Armhf but there is a demo which may help. You can find more information on the Community Document below (please download the attachment as it contains the document with instructions and some .deb files)&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/323514"&gt;https://community.nxp.com/message/323514&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 20:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Armhf-linux-for-iMX6ul-evk/m-p/996388#M147826</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-11-27T20:45:01Z</dc:date>
    </item>
  </channel>
</rss>