<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to setup debugging environment for image running in board?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-debugging-environment-for-image-running-in-board/m-p/995959#M147756</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with NXP iMX8QXPMEK evaluation board.&amp;nbsp; I downloaded bsp release L4.19.35_1.1.0_MX8QXP from following site:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="test_blank"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;BR /&gt;This bsp release is for Yocto Project 2.7 (Warrior)&lt;BR /&gt;I built yocto project for this bsp release.&amp;nbsp; I copied built image into sd card and then booted NXP board from sd card.&amp;nbsp; I need to step through USB Host Subsystem source code running in embedded linux kernel?&amp;nbsp; &lt;BR /&gt;There is a serial connection between my NXP evaluation board and my PC.&amp;nbsp; Micro-USB Debug port in NXP board is connected to USB port in my PC.&amp;nbsp; How do I setup debugging environment so I can see source code and symbols&lt;BR /&gt;running in my NXP board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Feb 2020 17:14:07 GMT</pubDate>
    <dc:creator>anaseem</dc:creator>
    <dc:date>2020-02-20T17:14:07Z</dc:date>
    <item>
      <title>How to setup debugging environment for image running in board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-debugging-environment-for-image-running-in-board/m-p/995959#M147756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with NXP iMX8QXPMEK evaluation board.&amp;nbsp; I downloaded bsp release L4.19.35_1.1.0_MX8QXP from following site:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="test_blank"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;BR /&gt;This bsp release is for Yocto Project 2.7 (Warrior)&lt;BR /&gt;I built yocto project for this bsp release.&amp;nbsp; I copied built image into sd card and then booted NXP board from sd card.&amp;nbsp; I need to step through USB Host Subsystem source code running in embedded linux kernel?&amp;nbsp; &lt;BR /&gt;There is a serial connection between my NXP evaluation board and my PC.&amp;nbsp; Micro-USB Debug port in NXP board is connected to USB port in my PC.&amp;nbsp; How do I setup debugging environment so I can see source code and symbols&lt;BR /&gt;running in my NXP board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2020 17:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-debugging-environment-for-image-running-in-board/m-p/995959#M147756</guid>
      <dc:creator>anaseem</dc:creator>
      <dc:date>2020-02-20T17:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup debugging environment for image running in board?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-debugging-environment-for-image-running-in-board/m-p/995960#M147757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general debug is described in AN12631&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12631.pdf" target="_blank"&gt;&lt;STRONG&gt;Normal and Secure Debug for i.MX8/8X Family of Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2020 23:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-setup-debugging-environment-for-image-running-in-board/m-p/995960#M147757</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-02-20T23:24:12Z</dc:date>
    </item>
  </channel>
</rss>