<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX 8M Mini TMU temperature readout problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995755#M147741</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The calibration values are in the efuses at:&lt;BR /&gt;0x4F0[7:0] TSENSOR_VALUE_RT[7:0] (room temp)&lt;BR /&gt;0x4F0[15:8] TSENSOR_VALUE_HT[7:0] (high temp)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Apr 2020 05:17:58 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-04-14T05:17:58Z</dc:date>
    <item>
      <title>i.MX 8M Mini TMU temperature readout problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995754#M147740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a new custom hardware using the i.MX 8M Mini SoC (commercial grade).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The temperature values reported by the TMU seem to be incorrect. At case temperatures of about 20°C ... 35 °C, I see the following values reported by U-Boot: 16°C, 18°C, 24°C, 28°C, 32°C, 36°C, 64°C, 72°C, 112°C.&lt;/P&gt;&lt;P&gt;Above 35°C, the temperature reading fails.&lt;/P&gt;&lt;P&gt;The same problem occurs within Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there some temperature calibration required for the TMU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ralf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 11:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995754#M147740</guid>
      <dc:creator>ralfgoebel</dc:creator>
      <dc:date>2020-03-20T11:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini TMU temperature readout problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995755#M147741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The calibration values are in the efuses at:&lt;BR /&gt;0x4F0[7:0] TSENSOR_VALUE_RT[7:0] (room temp)&lt;BR /&gt;0x4F0[15:8] TSENSOR_VALUE_HT[7:0] (high temp)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2020 05:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995755#M147741</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-04-14T05:17:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini TMU temperature readout problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995756#M147742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The efuse values for our boards are within the following ranges:&lt;/P&gt;&lt;P&gt;TSENSOR_VALUE_RT: 0x34 ... 0x39&lt;BR /&gt;TSENSOR_VALUE_HT: 0x69 ... 0x6f&lt;/P&gt;&lt;P&gt;Are they reasonable?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2020 10:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/995756#M147742</guid>
      <dc:creator>ralfgoebel</dc:creator>
      <dc:date>2020-04-14T10:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini TMU temperature readout problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/1480290#M191930</link>
      <description>&lt;P&gt;After comparing the circuit diagram of the i.MX8M Mini Reference Board with our implementation, we found that there is a 100k resistor to ground at pin TSENSOR_RES_EXT (J24). This pin is open on our board. Could this be the reason?&lt;BR /&gt;I found no documentation about this pin.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Ralf&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 06:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-TMU-temperature-readout-problem/m-p/1480290#M191930</guid>
      <dc:creator>ralfgoebel</dc:creator>
      <dc:date>2022-06-27T06:02:15Z</dc:date>
    </item>
  </channel>
</rss>