<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LTIB Error - RPM-FS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221892#M14752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes; it is very easy to build ready to use images and it is also very flexible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For iMX28 we have ready to use linux-3.7 with most hw supported so it might be good to test as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2013 18:28:35 GMT</pubDate>
    <dc:creator>OtavioSalvador</dc:creator>
    <dc:date>2013-01-11T18:28:35Z</dc:date>
    <item>
      <title>LTIB Error - RPM-FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221887#M14747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone help me with the LTIB for iMX28?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Ubuntu12.04 and I'm getting some error with rpm-fs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Processing platform: host support&lt;/P&gt;&lt;P&gt;===================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processing: rpm-fs&lt;/P&gt;&lt;P&gt;====================&lt;/P&gt;&lt;P&gt;ERROR: /tmp/rpm-gbrennon/RPMS/x86_64/rpm-fs-4.0.4-1.x86_64.rpm&lt;/P&gt;&lt;P&gt;would clobber '/reescale/ltib'&lt;/P&gt;&lt;P&gt;traceback:&lt;/P&gt;&lt;P&gt; main::check_host_clobber:2676&lt;/P&gt;&lt;P&gt;&amp;nbsp; main::build_rpm:906&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; main::f_buildrpms:980&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; main::check_rpm_setup:2407&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; main::host_checks:1423&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; main:542&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Started: Tue Jan&amp;nbsp; 8 15:26:08 2013&lt;/P&gt;&lt;P&gt;Ended:&amp;nbsp;&amp;nbsp; Tue Jan&amp;nbsp; 8 15:26:09 2013&lt;/P&gt;&lt;P&gt;Elapsed: 1 seconds&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;"&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2013 17:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221887#M14747</guid>
      <dc:creator>gláuberazevedo</dc:creator>
      <dc:date>2013-01-08T17:28:51Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB Error - RPM-FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221888#M14748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gláuberazevedo"&gt;gláuberazevedo&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not a LTIB user but a Yocto developer and I'd like to ask you to give a try in Yocto. It provides full support for newer host distributions and has a very updated software stack. We have add support for mx28evk and it should be easy for you to give it a try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check more at &lt;A href="https://github.com/Freescale/fsl-community-bsp-platform" title="https://github.com/Freescale/fsl-community-bsp-platform"&gt;Freescale/fsl-community-bsp-platform · GitHub&lt;/A&gt; as it has a small documentation how to start. If you want to learn more about Yocto itself you can learn more at &lt;A href="https://www.yoctoproject.org/documentation/current" title="https://www.yoctoproject.org/documentation/current"&gt;https://www.yoctoproject.org/documentation/current&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 15:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221888#M14748</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2013-01-10T15:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB Error - RPM-FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221889#M14749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gláuber ,&lt;/P&gt;&lt;P&gt;I would often find that LTIB would fail because I needed to install a required package. After installing the missing package LTIB would fail as you saw because it refused to overwrite a file it had created on the previous attempt. Just delete the entire LTIB created file structure and start from scratch.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 19:46:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221889#M14749</guid>
      <dc:creator>MichaelOConnor</dc:creator>
      <dc:date>2013-01-10T19:46:42Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB Error - RPM-FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221890#M14750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following link will be useful to you. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-1442" title="https://community.freescale.com/docs/DOC-1442"&gt;https://community.freescale.com/docs/DOC-1442&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2013 03:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221890#M14750</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2013-01-11T03:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB Error - RPM-FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221891#M14751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As Otavio pointed out I would recommend you take a look at Yocto.&amp;nbsp; I was able to get the Yocto build system running on Ubuntu 12.04 without issue.&amp;nbsp; Just follow the Yocto Quick Start guide.&amp;nbsp; The meta-fsl-arm build for the MX53 built without issue and booted right up.&amp;nbsp; I plan on testing the MX28 soon as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2013 18:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221891#M14751</guid>
      <dc:creator>everlook</dc:creator>
      <dc:date>2013-01-11T18:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB Error - RPM-FS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221892#M14752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes; it is very easy to build ready to use images and it is also very flexible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For iMX28 we have ready to use linux-3.7 with most hw supported so it might be good to test as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2013 18:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-Error-RPM-FS/m-p/221892#M14752</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2013-01-11T18:28:35Z</dc:date>
    </item>
  </channel>
</rss>