<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADV7282-m NTSC issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ADV7282-m-NTSC-issue/m-p/992942#M147318</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the topic as below, check if you set register or source code correct or not&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/303792#comment-314760" title="https://community.nxp.com/thread/303792#comment-314760"&gt;https://community.nxp.com/thread/303792#comment-314760&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://ez.analog.com/video/f/q-a/8004/cannot-capture-from-adv7281-m-with-i-mx6q" title="https://ez.analog.com/video/f/q-a/8004/cannot-capture-from-adv7281-m-with-i-mx6q"&gt;Cannot capture from ADV7281-M with i.MX6Q - Q&amp;amp;A - Video - EngineerZone&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2019 07:55:49 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2019-11-21T07:55:49Z</dc:date>
    <item>
      <title>ADV7282-m NTSC issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADV7282-m-NTSC-issue/m-p/992941#M147317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We build a custom board with an ADV7282-M video grabber and I'm trying to get it to work. I followed&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/434286"&gt;this&lt;/A&gt; and &lt;A _jive_internal="true" href="https://community.nxp.com/thread/434697"&gt;this&lt;/A&gt; post to get a driver working and to configure the device tree. This works up to a point. I have a working driver, I can stream video using gstreamer and it automatically detects PAL/NTSC. However when I connect a NTSC camera and start the stream the image sometimes is scrolling vertically. This happens about 50% of the time. When connecting a PAL camera all seems to work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both cases I continually get the following error:&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I modify the .active_top = 13 setting in mxc_v4l2_capture.c to for example 14 the scrolling goes from top to bottom (and seems to occur less often). I read a lot of forum posts about this issue but cant figure out the exact problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another thing is when I switch camera while streaming the image gets out of sync (horizontally and/or vertically) and never recovers. What I read so far tells me that I have to use STREAMON/STREAMOFF ioctl calls to fix this, is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone point me in the right direction? I'm new to IPU and CSI configuration so I'm having a hard time figuring this out.&lt;/P&gt;&lt;P&gt;If more information is needed feel free to ask.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rens&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Nov 2019 14:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADV7282-m-NTSC-issue/m-p/992941#M147317</guid>
      <dc:creator>rens</dc:creator>
      <dc:date>2019-11-14T14:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: ADV7282-m NTSC issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADV7282-m-NTSC-issue/m-p/992942#M147318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the topic as below, check if you set register or source code correct or not&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/303792#comment-314760" title="https://community.nxp.com/thread/303792#comment-314760"&gt;https://community.nxp.com/thread/303792#comment-314760&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://ez.analog.com/video/f/q-a/8004/cannot-capture-from-adv7281-m-with-i-mx6q" title="https://ez.analog.com/video/f/q-a/8004/cannot-capture-from-adv7281-m-with-i-mx6q"&gt;Cannot capture from ADV7281-M with i.MX6Q - Q&amp;amp;A - Video - EngineerZone&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 07:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADV7282-m-NTSC-issue/m-p/992942#M147318</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-11-21T07:55:49Z</dc:date>
    </item>
  </channel>
</rss>