<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8M Mini suspend mode issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-suspend-mode-issue/m-p/990413#M147013</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an imx8m mini development board with pca9450(PMIC) and&amp;nbsp; DDR3L. We use the following command to put it into suspend mode, but we cannot wake it up through the serial port(Debug port).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo enabled &amp;gt; /sys/class/tty/ttymxc1/power/wakeup&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo mem &amp;gt; /sys/power/state&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103829iFE99BEA9E07050FA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In suspend mode, the&amp;nbsp;VDD_ARM&amp;nbsp; voltage is 0V, NVCC_DRAM is 1.35V, VDD_SOC is 0.8V,VDD_GPU is 0.75V.&lt;/P&gt;&lt;P&gt;After entering any characters into the serial port,&amp;nbsp;&lt;SPAN&gt;the&amp;nbsp;VDD_ARM&amp;nbsp; voltage is 0.9V, NVCC_DRAM is 1.35V, VDD_SOC is 0.85V,VDD_GPU is 0.95V.But the system hangs and no characters are output from the debug port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How should we debug about resuming from suspend mode?&lt;/P&gt;&lt;P&gt;Is there any relevant guidance material?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2020 08:26:42 GMT</pubDate>
    <dc:creator>baijinlong</dc:creator>
    <dc:date>2020-03-19T08:26:42Z</dc:date>
    <item>
      <title>i.MX 8M Mini suspend mode issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-suspend-mode-issue/m-p/990413#M147013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an imx8m mini development board with pca9450(PMIC) and&amp;nbsp; DDR3L. We use the following command to put it into suspend mode, but we cannot wake it up through the serial port(Debug port).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo enabled &amp;gt; /sys/class/tty/ttymxc1/power/wakeup&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo mem &amp;gt; /sys/power/state&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103829iFE99BEA9E07050FA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In suspend mode, the&amp;nbsp;VDD_ARM&amp;nbsp; voltage is 0V, NVCC_DRAM is 1.35V, VDD_SOC is 0.8V,VDD_GPU is 0.75V.&lt;/P&gt;&lt;P&gt;After entering any characters into the serial port,&amp;nbsp;&lt;SPAN&gt;the&amp;nbsp;VDD_ARM&amp;nbsp; voltage is 0.9V, NVCC_DRAM is 1.35V, VDD_SOC is 0.85V,VDD_GPU is 0.95V.But the system hangs and no characters are output from the debug port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How should we debug about resuming from suspend mode?&lt;/P&gt;&lt;P&gt;Is there any relevant guidance material?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 08:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-suspend-mode-issue/m-p/990413#M147013</guid>
      <dc:creator>baijinlong</dc:creator>
      <dc:date>2020-03-19T08:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini suspend mode issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-suspend-mode-issue/m-p/990414#M147014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jinlong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems board just hanged (probably due to custom board software modifications)&lt;/P&gt;&lt;P&gt;based on provided data (in particular "VDD_GPU is 0.75V" compared with data provided in&lt;/P&gt;&lt;P&gt;Table 2. Suspend mode&amp;nbsp; &lt;A href="https://www.nxp.com/docs/en/application-note/AN12410.pdf" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Mini Power Consumption Measurement &lt;/STRONG&gt;&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;Suspend mode can be tested on reference board with Demo Images from link&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/i-mx-developer-resources/i-mx-software-and-development-tools:IMX-SW" title="https://www.nxp.com/design/i-mx-developer-resources/i-mx-software-and-development-tools:IMX-SW"&gt;i.MX Software and Development Tools | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 03:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-suspend-mode-issue/m-p/990414#M147014</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-03-20T03:05:32Z</dc:date>
    </item>
  </channel>
</rss>