<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX6QP LPDDR2 Calibration Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QP-LPDDR2-Calibration-Issue/m-p/988006#M146688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We need some help for iMX6QP LPDDR2 Dual-channel bringing up. Here are details below.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Board ID: SCH-29181 REV B&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;DDR Device: Micron - EDBA164B2PR&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Programming aids:&amp;nbsp;MX6QP_SabreSD_LPDDR2_register_programming_aid_v1_3&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;DDR stress tester: V3.0&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We have generated initial file 6QP.inc from aids, which only changed tMRD and some pad resistance, and we use 2 channel, 2 cs per channel.&amp;nbsp; MR1 Value(HEX)=C201&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Now, channel 0 can calibrate successfully at 400MHz, but channel 1 fail calibration from 300 to 400. Any can give some help?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR Stress Test (3.0.0) &lt;BR /&gt; Build: Dec 14 2018, 14:12:06&lt;BR /&gt; NXP Semiconductors.&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Dual/Quad (0x63)&lt;BR /&gt;Internal Revision = TO2.0&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00100000&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x12000000&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x01, Fixed 2x32 map.&lt;BR /&gt;DDR type is LPDDR2 in 2-channel fixed 2x32 mode. Showing channel0 info only&lt;BR /&gt;Data width: 32, bank num: 8&lt;BR /&gt;Row size: 14, col size: 10&lt;BR /&gt;Both chip select CSD0 and CSD1 are used &lt;BR /&gt;Density per chip select: 512MB &lt;BR /&gt;Density per channel: 1024MB&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;NOTE:In order to run calibration in LPDDR2 2-channel fixed 2x32 mode both (all) &lt;BR /&gt; channels must be selected to test, if not, calibration will fail requiring you &lt;BR /&gt; to re-start the test. You can also choose to skip calibration. &lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Current Temperature: 27&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;DDR Freq: 396 MHz&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;LPDDR2 2 CHANNELS&lt;BR /&gt;Note: Array result[] holds the DRAM test result of each byte. &lt;BR /&gt; 0: test pass. 1: test fail &lt;BR /&gt; 4 bits respresent the result of 1 byte. &lt;BR /&gt; result 0001:byte 0 fail. &lt;BR /&gt; result 0011:byte 0, 1 fail.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Starting Read calibration...&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Test channel 0&lt;BR /&gt;ABS_OFFSET=0x00000000 result[00]=0x1111&lt;BR /&gt;ABS_OFFSET=0x04040404 result[01]=0x1111&lt;BR /&gt;ABS_OFFSET=0x08080808 result[02]=0x1111&lt;BR /&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x1111&lt;BR /&gt;ABS_OFFSET=0x10101010 result[04]=0x1111&lt;BR /&gt;ABS_OFFSET=0x14141414 result[05]=0x1111&lt;BR /&gt;ABS_OFFSET=0x18181818 result[06]=0x1000&lt;BR /&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x0000&lt;BR /&gt;ABS_OFFSET=0x20202020 result[08]=0x0010&lt;BR /&gt;ABS_OFFSET=0x24242424 result[09]=0x0000&lt;BR /&gt;ABS_OFFSET=0x28282828 result[0A]=0x0010&lt;BR /&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x0000&lt;BR /&gt;ABS_OFFSET=0x30303030 result[0C]=0x0000&lt;BR /&gt;ABS_OFFSET=0x34343434 result[0D]=0x0000&lt;BR /&gt;ABS_OFFSET=0x38383838 result[0E]=0x0000&lt;BR /&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x0000&lt;BR /&gt;ABS_OFFSET=0x40404040 result[10]=0x0000&lt;BR /&gt;ABS_OFFSET=0x44444444 result[11]=0x0010&lt;BR /&gt;ABS_OFFSET=0x48484848 result[12]=0x0000&lt;BR /&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x0000&lt;BR /&gt;ABS_OFFSET=0x50505050 result[14]=0x0000&lt;BR /&gt;ABS_OFFSET=0x54545454 result[15]=0x0000&lt;BR /&gt;ABS_OFFSET=0x58585858 result[16]=0x0000&lt;BR /&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x0000&lt;BR /&gt;ABS_OFFSET=0x60606060 result[18]=0x0000&lt;BR /&gt;ABS_OFFSET=0x64646464 result[19]=0x0000&lt;BR /&gt;ABS_OFFSET=0x68686868 result[1A]=0x0010&lt;BR /&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x0111&lt;BR /&gt;ABS_OFFSET=0x70707070 result[1C]=0x0111&lt;BR /&gt;ABS_OFFSET=0x74747474 result[1D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x78787878 result[1E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Byte 0: (0x18 - 0x68), middle value:0x40&lt;BR /&gt;Byte 1: (0x48 - 0x64), middle value:0x56&lt;BR /&gt;Byte 2: (0x18 - 0x68), middle value:0x40&lt;BR /&gt;Byte 3: (0x1c - 0x70), middle value:0x46&lt;BR /&gt;Test channel 1&lt;BR /&gt;ABS_OFFSET=0x00000000 result[00]=0x1111&lt;BR /&gt;ABS_OFFSET=0x04040404 result[01]=0x1111&lt;BR /&gt;ABS_OFFSET=0x08080808 result[02]=0x1111&lt;BR /&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x1111&lt;BR /&gt;ABS_OFFSET=0x10101010 result[04]=0x1111&lt;BR /&gt;ABS_OFFSET=0x14141414 result[05]=0x1111&lt;BR /&gt;ABS_OFFSET=0x18181818 result[06]=0x1111&lt;BR /&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x1111&lt;BR /&gt;ABS_OFFSET=0x20202020 result[08]=0x1111&lt;BR /&gt;ABS_OFFSET=0x24242424 result[09]=0x1111&lt;BR /&gt;ABS_OFFSET=0x28282828 result[0A]=0x1111&lt;BR /&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x1111&lt;BR /&gt;ABS_OFFSET=0x30303030 result[0C]=0x1111&lt;BR /&gt;ABS_OFFSET=0x34343434 result[0D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x38383838 result[0E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x1111&lt;BR /&gt;ABS_OFFSET=0x40404040 result[10]=0x1111&lt;BR /&gt;ABS_OFFSET=0x44444444 result[11]=0x1111&lt;BR /&gt;ABS_OFFSET=0x48484848 result[12]=0x1111&lt;BR /&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x1111&lt;BR /&gt;ABS_OFFSET=0x50505050 result[14]=0x1111&lt;BR /&gt;ABS_OFFSET=0x54545454 result[15]=0x1111&lt;BR /&gt;ABS_OFFSET=0x58585858 result[16]=0x1111&lt;BR /&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x1111&lt;BR /&gt;ABS_OFFSET=0x60606060 result[18]=0x1111&lt;BR /&gt;ABS_OFFSET=0x64646464 result[19]=0x1111&lt;BR /&gt;ABS_OFFSET=0x68686868 result[1A]=0x1111&lt;BR /&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111&lt;BR /&gt;ABS_OFFSET=0x70707070 result[1C]=0x1111&lt;BR /&gt;ABS_OFFSET=0x74747474 result[1D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x78787878 result[1E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;ERROR FOUND, we can't get suitable value !!!!&lt;BR /&gt;dram test fails for all values.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Error: failed during ddr calibration&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Oct 2019 03:34:03 GMT</pubDate>
    <dc:creator>nxf53093</dc:creator>
    <dc:date>2019-10-31T03:34:03Z</dc:date>
    <item>
      <title>IMX6QP LPDDR2 Calibration Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QP-LPDDR2-Calibration-Issue/m-p/988006#M146688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We need some help for iMX6QP LPDDR2 Dual-channel bringing up. Here are details below.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Board ID: SCH-29181 REV B&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;DDR Device: Micron - EDBA164B2PR&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Programming aids:&amp;nbsp;MX6QP_SabreSD_LPDDR2_register_programming_aid_v1_3&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;DDR stress tester: V3.0&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We have generated initial file 6QP.inc from aids, which only changed tMRD and some pad resistance, and we use 2 channel, 2 cs per channel.&amp;nbsp; MR1 Value(HEX)=C201&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Now, channel 0 can calibrate successfully at 400MHz, but channel 1 fail calibration from 300 to 400. Any can give some help?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR Stress Test (3.0.0) &lt;BR /&gt; Build: Dec 14 2018, 14:12:06&lt;BR /&gt; NXP Semiconductors.&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Dual/Quad (0x63)&lt;BR /&gt;Internal Revision = TO2.0&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00100000&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x12000000&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x01, Fixed 2x32 map.&lt;BR /&gt;DDR type is LPDDR2 in 2-channel fixed 2x32 mode. Showing channel0 info only&lt;BR /&gt;Data width: 32, bank num: 8&lt;BR /&gt;Row size: 14, col size: 10&lt;BR /&gt;Both chip select CSD0 and CSD1 are used &lt;BR /&gt;Density per chip select: 512MB &lt;BR /&gt;Density per channel: 1024MB&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;NOTE:In order to run calibration in LPDDR2 2-channel fixed 2x32 mode both (all) &lt;BR /&gt; channels must be selected to test, if not, calibration will fail requiring you &lt;BR /&gt; to re-start the test. You can also choose to skip calibration. &lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Current Temperature: 27&lt;BR /&gt;============================================&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;DDR Freq: 396 MHz&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;LPDDR2 2 CHANNELS&lt;BR /&gt;Note: Array result[] holds the DRAM test result of each byte. &lt;BR /&gt; 0: test pass. 1: test fail &lt;BR /&gt; 4 bits respresent the result of 1 byte. &lt;BR /&gt; result 0001:byte 0 fail. &lt;BR /&gt; result 0011:byte 0, 1 fail.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Starting Read calibration...&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Test channel 0&lt;BR /&gt;ABS_OFFSET=0x00000000 result[00]=0x1111&lt;BR /&gt;ABS_OFFSET=0x04040404 result[01]=0x1111&lt;BR /&gt;ABS_OFFSET=0x08080808 result[02]=0x1111&lt;BR /&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x1111&lt;BR /&gt;ABS_OFFSET=0x10101010 result[04]=0x1111&lt;BR /&gt;ABS_OFFSET=0x14141414 result[05]=0x1111&lt;BR /&gt;ABS_OFFSET=0x18181818 result[06]=0x1000&lt;BR /&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x0000&lt;BR /&gt;ABS_OFFSET=0x20202020 result[08]=0x0010&lt;BR /&gt;ABS_OFFSET=0x24242424 result[09]=0x0000&lt;BR /&gt;ABS_OFFSET=0x28282828 result[0A]=0x0010&lt;BR /&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x0000&lt;BR /&gt;ABS_OFFSET=0x30303030 result[0C]=0x0000&lt;BR /&gt;ABS_OFFSET=0x34343434 result[0D]=0x0000&lt;BR /&gt;ABS_OFFSET=0x38383838 result[0E]=0x0000&lt;BR /&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x0000&lt;BR /&gt;ABS_OFFSET=0x40404040 result[10]=0x0000&lt;BR /&gt;ABS_OFFSET=0x44444444 result[11]=0x0010&lt;BR /&gt;ABS_OFFSET=0x48484848 result[12]=0x0000&lt;BR /&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x0000&lt;BR /&gt;ABS_OFFSET=0x50505050 result[14]=0x0000&lt;BR /&gt;ABS_OFFSET=0x54545454 result[15]=0x0000&lt;BR /&gt;ABS_OFFSET=0x58585858 result[16]=0x0000&lt;BR /&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x0000&lt;BR /&gt;ABS_OFFSET=0x60606060 result[18]=0x0000&lt;BR /&gt;ABS_OFFSET=0x64646464 result[19]=0x0000&lt;BR /&gt;ABS_OFFSET=0x68686868 result[1A]=0x0010&lt;BR /&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x0111&lt;BR /&gt;ABS_OFFSET=0x70707070 result[1C]=0x0111&lt;BR /&gt;ABS_OFFSET=0x74747474 result[1D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x78787878 result[1E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Byte 0: (0x18 - 0x68), middle value:0x40&lt;BR /&gt;Byte 1: (0x48 - 0x64), middle value:0x56&lt;BR /&gt;Byte 2: (0x18 - 0x68), middle value:0x40&lt;BR /&gt;Byte 3: (0x1c - 0x70), middle value:0x46&lt;BR /&gt;Test channel 1&lt;BR /&gt;ABS_OFFSET=0x00000000 result[00]=0x1111&lt;BR /&gt;ABS_OFFSET=0x04040404 result[01]=0x1111&lt;BR /&gt;ABS_OFFSET=0x08080808 result[02]=0x1111&lt;BR /&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x1111&lt;BR /&gt;ABS_OFFSET=0x10101010 result[04]=0x1111&lt;BR /&gt;ABS_OFFSET=0x14141414 result[05]=0x1111&lt;BR /&gt;ABS_OFFSET=0x18181818 result[06]=0x1111&lt;BR /&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x1111&lt;BR /&gt;ABS_OFFSET=0x20202020 result[08]=0x1111&lt;BR /&gt;ABS_OFFSET=0x24242424 result[09]=0x1111&lt;BR /&gt;ABS_OFFSET=0x28282828 result[0A]=0x1111&lt;BR /&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x1111&lt;BR /&gt;ABS_OFFSET=0x30303030 result[0C]=0x1111&lt;BR /&gt;ABS_OFFSET=0x34343434 result[0D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x38383838 result[0E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x1111&lt;BR /&gt;ABS_OFFSET=0x40404040 result[10]=0x1111&lt;BR /&gt;ABS_OFFSET=0x44444444 result[11]=0x1111&lt;BR /&gt;ABS_OFFSET=0x48484848 result[12]=0x1111&lt;BR /&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x1111&lt;BR /&gt;ABS_OFFSET=0x50505050 result[14]=0x1111&lt;BR /&gt;ABS_OFFSET=0x54545454 result[15]=0x1111&lt;BR /&gt;ABS_OFFSET=0x58585858 result[16]=0x1111&lt;BR /&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x1111&lt;BR /&gt;ABS_OFFSET=0x60606060 result[18]=0x1111&lt;BR /&gt;ABS_OFFSET=0x64646464 result[19]=0x1111&lt;BR /&gt;ABS_OFFSET=0x68686868 result[1A]=0x1111&lt;BR /&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111&lt;BR /&gt;ABS_OFFSET=0x70707070 result[1C]=0x1111&lt;BR /&gt;ABS_OFFSET=0x74747474 result[1D]=0x1111&lt;BR /&gt;ABS_OFFSET=0x78787878 result[1E]=0x1111&lt;BR /&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;ERROR FOUND, we can't get suitable value !!!!&lt;BR /&gt;dram test fails for all values.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Error: failed during ddr calibration&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2019 03:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6QP-LPDDR2-Calibration-Issue/m-p/988006#M146688</guid>
      <dc:creator>nxf53093</dc:creator>
      <dc:date>2019-10-31T03:34:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6QP LPDDR2 Calibration Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QP-LPDDR2-Calibration-Issue/m-p/988007#M146689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Are there differences in PCB layout for the LPDDR2 channels? &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Also, customers can use the following aid tool:&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/docs/DOC-95089"&gt;https://community.nxp.com/docs/DOC-95089&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2019 08:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6QP-LPDDR2-Calibration-Issue/m-p/988007#M146689</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-11-05T08:27:07Z</dc:date>
    </item>
  </channel>
</rss>