<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Need continuous BCLK?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Need-continuous-BCLK/m-p/987864#M146665</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-userid="23351" data-username="sparkyee" href="https://community.nxp.com/people/sparkyee"&gt;Larry&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;see below, please!&lt;/P&gt;&lt;P&gt;(1) About EIM_BLCK&lt;/P&gt;&lt;P&gt;yes, the clock can be configured as continous in register EIM_WCR&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104700iFDF60E51AA758142/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;more detailed information ,see reference manual, please!&lt;/P&gt;&lt;P&gt;(2) Suggestion on clock for your FPGA's working clock&lt;/P&gt;&lt;P&gt;--- provided by CPU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The better choice is to get clock from CCM_CLKO1 &amp;amp; CCM_CLKO2.&lt;/P&gt;&lt;P&gt;--- Using external clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; probably FPGA requires higher precision clock, From a technical point of view, you can choose to meet the requirements of OSC or crystal, which has no risk.&lt;/P&gt;&lt;P&gt;(3) Signal transmission synchronous clock&lt;/P&gt;&lt;P&gt;If your FPGA is connected to EIM interface and use SYNC mode, it is no problem to use BLCK for FPGA.&amp;nbsp; It is not recommended that you use BCLK as the working clock of FPGA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jan 2020 04:10:17 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2020-01-10T04:10:17Z</dc:date>
    <item>
      <title>Need continuous BCLK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-continuous-BCLK/m-p/987863#M146664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am designing a product using the iMX6ULL. I need a clock to run my FPGA and cannot use&lt;/P&gt;&lt;P&gt;CCM Clock 1 or 2 since I am using SD card port 1 and I need the JTAG port operable. I am&lt;/P&gt;&lt;P&gt;thinking of using EIM "BCLK" and have found the "CONT_BCLK_SEL" bit in the EIM_WCR register.&lt;/P&gt;&lt;P&gt;There seems to be a lot of discussion in the community whether BCLK can function like one of the&lt;/P&gt;&lt;P&gt;CCM_CLK, this is possible? Will it work for my&amp;nbsp;MCIMX6Y2CVM08AB part? I would like to test this&lt;/P&gt;&lt;P&gt;signal on my Freescale iMX6ULL-EVK and would also like to know how to change the UBOOT/ LINUX&lt;/P&gt;&lt;P&gt;software to accomplish this function from startup? If "BCLK"&amp;nbsp; is not continuously possible can you suggest&lt;/P&gt;&lt;P&gt;any other means of getting a continuous clock for the iMX6ULL part?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reading and helping!&lt;/P&gt;&lt;P&gt;Larry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2020 14:46:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-continuous-BCLK/m-p/987863#M146664</guid>
      <dc:creator>sparkyee</dc:creator>
      <dc:date>2020-01-09T14:46:53Z</dc:date>
    </item>
    <item>
      <title>Re: Need continuous BCLK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-continuous-BCLK/m-p/987864#M146665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-userid="23351" data-username="sparkyee" href="https://community.nxp.com/people/sparkyee"&gt;Larry&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;see below, please!&lt;/P&gt;&lt;P&gt;(1) About EIM_BLCK&lt;/P&gt;&lt;P&gt;yes, the clock can be configured as continous in register EIM_WCR&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104700iFDF60E51AA758142/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;more detailed information ,see reference manual, please!&lt;/P&gt;&lt;P&gt;(2) Suggestion on clock for your FPGA's working clock&lt;/P&gt;&lt;P&gt;--- provided by CPU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The better choice is to get clock from CCM_CLKO1 &amp;amp; CCM_CLKO2.&lt;/P&gt;&lt;P&gt;--- Using external clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; probably FPGA requires higher precision clock, From a technical point of view, you can choose to meet the requirements of OSC or crystal, which has no risk.&lt;/P&gt;&lt;P&gt;(3) Signal transmission synchronous clock&lt;/P&gt;&lt;P&gt;If your FPGA is connected to EIM interface and use SYNC mode, it is no problem to use BLCK for FPGA.&amp;nbsp; It is not recommended that you use BCLK as the working clock of FPGA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2020 04:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-continuous-BCLK/m-p/987864#M146665</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-01-10T04:10:17Z</dc:date>
    </item>
  </channel>
</rss>