<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987568#M146642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on &lt;STRONG&gt;imx8qm-mek&lt;/STRONG&gt; running on &lt;STRONG&gt;Android 9 - auto&lt;/STRONG&gt;. I have gone through the couple of posts from this forum regarding HDMI-RX functionality.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used&amp;nbsp;fsl-imx8qm-mek-hdmi-in.dts as reference and modified&amp;nbsp;fsl-imx8qm-mek-car.dts. After flashing completed build on MEK platform&amp;nbsp; i am receiving below log.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[ 4.424144] [drm:hdmirx_init] *ERROR* NO HDMI RX FW running&lt;BR /&gt;[ 4.429740] mxc-hdmi-rx 58268000.hdmi_rx: mxc hdmi rx init failed&lt;BR /&gt;s[ 4.435919] mxc-hdmi-rx 58268000.hdmi_rx: mxc hdmi rx probe failed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;So here i see that HDMI RX FW is not running and so the error is thrown.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found the firmware are locate here :&amp;nbsp;&lt;/P&gt;&lt;P&gt;vendor/nxp/linux-firmware-imx/firmware/hdmi/cadence/hdmirxfw.bin&amp;nbsp;&lt;/P&gt;&lt;P&gt;vendor/nxp-opensource/imx-mkimage/iMX8QM/hdmirxfw.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to understand how i can use these firmware to resolve the above issue ? It will be great if someone can throw some light here.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2020 13:19:19 GMT</pubDate>
    <dc:creator>amit251291</dc:creator>
    <dc:date>2020-03-19T13:19:19Z</dc:date>
    <item>
      <title>HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987568#M146642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on &lt;STRONG&gt;imx8qm-mek&lt;/STRONG&gt; running on &lt;STRONG&gt;Android 9 - auto&lt;/STRONG&gt;. I have gone through the couple of posts from this forum regarding HDMI-RX functionality.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used&amp;nbsp;fsl-imx8qm-mek-hdmi-in.dts as reference and modified&amp;nbsp;fsl-imx8qm-mek-car.dts. After flashing completed build on MEK platform&amp;nbsp; i am receiving below log.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[ 4.424144] [drm:hdmirx_init] *ERROR* NO HDMI RX FW running&lt;BR /&gt;[ 4.429740] mxc-hdmi-rx 58268000.hdmi_rx: mxc hdmi rx init failed&lt;BR /&gt;s[ 4.435919] mxc-hdmi-rx 58268000.hdmi_rx: mxc hdmi rx probe failed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;So here i see that HDMI RX FW is not running and so the error is thrown.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found the firmware are locate here :&amp;nbsp;&lt;/P&gt;&lt;P&gt;vendor/nxp/linux-firmware-imx/firmware/hdmi/cadence/hdmirxfw.bin&amp;nbsp;&lt;/P&gt;&lt;P&gt;vendor/nxp-opensource/imx-mkimage/iMX8QM/hdmirxfw.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to understand how i can use these firmware to resolve the above issue ? It will be great if someone can throw some light here.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 13:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987568#M146642</guid>
      <dc:creator>amit251291</dc:creator>
      <dc:date>2020-03-19T13:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987569#M146643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;image should have correct signed HDMI RX firmware, however according&lt;/P&gt;&lt;P&gt;to p.21 &lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX8QMAEC.pdf" target="_blank"&gt;&lt;STRONG&gt;i.MX 8QuadMax Automotive and Infotainment Applications Processors&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;currently HDMI RX is not supported, relevant software and documentation may be provided later&lt;/P&gt;&lt;P&gt;after validation.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98205iA5B20240D34DCF1F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 10:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987569#M146643</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-03-20T10:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987570#M146644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you&amp;nbsp;&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;‌ for your response.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Apr 2020 06:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/987570#M146644</guid>
      <dc:creator>amit251291</dc:creator>
      <dc:date>2020-04-03T06:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI RX or HDMI-IN on imx8qm-mek with Android 9 Auto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/1174663#M164198</link>
      <description>&lt;P&gt;Dear Igor, what is the current status of HDMI Rx?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nikolaj&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 17:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-RX-or-HDMI-IN-on-imx8qm-mek-with-Android-9-Auto/m-p/1174663#M164198</guid>
      <dc:creator>nhermann</dc:creator>
      <dc:date>2020-10-28T17:09:40Z</dc:date>
    </item>
  </channel>
</rss>