<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Capture image issues with IMX7D and CSI (CMOS)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987564#M146640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor, I checked the source for mx6s_v4l2_capture.out on the link you provided and it still uses .&lt;SPAN class=""&gt;enum_mbus_fmt&amp;nbsp;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Do you know if mxc_v4l2_capture.c is compatible with imx7d CSI and can be used instead?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jan 2020 23:41:17 GMT</pubDate>
    <dc:creator>eddie_vazquez_h</dc:creator>
    <dc:date>2020-01-21T23:41:17Z</dc:date>
    <item>
      <title>Capture image issues with IMX7D and CSI (CMOS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987562#M146638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community, &lt;/P&gt;&lt;P&gt;I have several questions regarding capturing a single picture using CSI interface. I have set up parallel sensor and csi driver (mx6s_capture.c). Driver for camera was ported to use subdev and succesfully shows as subdev of csi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to use &lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;./mx6s_v4l2_capture.out -d /dev/video0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It calls functions from sensor driver but throws the following error:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;VIDIOC ENUM FMT failed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Comparing my&amp;nbsp; /include/media/v4l2-subdev.h against an older copy, the .&lt;SPAN class=""&gt;enum_mbus_fmt&lt;/SPAN&gt; in v4l2_subdev_video_ops is gone so I'm thinking maybe mx6s_v4l2_capture.out it's outdated. Do you have a newer version for this tool and also some documentation on how to use it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I've noticed csi_enable function in mx6s_capture.c never gets called and hence peripheral is never enabled. How could I call this function from user space? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In a nutshell all I'm pursuing is to take a picture (no video), no matter if from user space or programatically, do you have any documentation or thread on how to accomplish this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 20:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987562#M146638</guid>
      <dc:creator>eddie_vazquez_h</dc:creator>
      <dc:date>2020-01-21T20:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: Capture image issues with IMX7D and CSI (CMOS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987563#M146639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eddie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with latest csi unit tests&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test?h=imx_4.19.35_1.1.0"&gt;mxc_v4l2_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and &lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_LINUX_DOCS" target="_blank"&gt;Linux 4.19.35_1.1.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 23:20:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987563#M146639</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-21T23:20:15Z</dc:date>
    </item>
    <item>
      <title>Re: Capture image issues with IMX7D and CSI (CMOS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987564#M146640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor, I checked the source for mx6s_v4l2_capture.out on the link you provided and it still uses .&lt;SPAN class=""&gt;enum_mbus_fmt&amp;nbsp;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Do you know if mxc_v4l2_capture.c is compatible with imx7d CSI and can be used instead?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 23:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987564#M146640</guid>
      <dc:creator>eddie_vazquez_h</dc:creator>
      <dc:date>2020-01-21T23:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: Capture image issues with IMX7D and CSI (CMOS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987565#M146641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes it is compatible and can be debugged as on link&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/375865"&gt;About preview function in i.MX6SL.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2020 06:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-image-issues-with-IMX7D-and-CSI-CMOS/m-p/987565#M146641</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-22T06:18:24Z</dc:date>
    </item>
  </channel>
</rss>