<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Excellent Dev Kit Deal for iMX53 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221499#M14657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I came across a great deal on a iMX53 based dev kit that I thought others might also be interested in it. Digi is offering a iMX53 Jumpstart Kit (CC-WMX53-ANDRD) for Android for $199.&amp;nbsp; It is a complete kit and includes a nice 7" LCD (with touch).&amp;nbsp; Here are some details:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;ConnectCore Wi-i.MX53 module&lt;BR /&gt; - 1 GHz i.MX53, 512 MB NAND Flash, 512 MB DDR2, -20 to +70° C&lt;/LI&gt;&lt;LI&gt;7" WVGA LCD panel with touchscreen&lt;/LI&gt;&lt;LI&gt;Digi JumpStart Kit development board &lt;BR /&gt; 3 serial ports (1 x RS-232/422/485, 1 x RS-232 Tx/Rx, 1 x TTL), VGA, HDMI 1.3, Ethernet (RJ-45), WLAN antenna connectors, SD/MMC slot, MicroSD slot, USB OTG, 4 x USB Host, I2C/SPI headers, 1-Wire connector, audio: line in/out and microphone in (3.5 mm), Digi XBee module socket module sold separately), GPIO screw terminal, user push-buttons, user LEDs, battery, 802.3af (PoE) module socket (module sold separately), external LCD/Touchscreen connectors, external camera connectors, user/application connectors, JTAG connector, 9-30VDC power supply, power switch&lt;/LI&gt;&lt;LI&gt;Power supply and accessories&lt;BR /&gt; - External wall power supply with adapters,&lt;BR /&gt; Ethernet cable, antennas, serial cable&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I just received mine yesterday and so I have not had too much time to play with it, other than just turning it on... it looks like I will be busy this weekend..&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Cheers,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;Sam&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 20 Oct 2012 14:40:56 GMT</pubDate>
    <dc:creator>samsaprunoff</dc:creator>
    <dc:date>2012-10-20T14:40:56Z</dc:date>
    <item>
      <title>Excellent Dev Kit Deal for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221499#M14657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I came across a great deal on a iMX53 based dev kit that I thought others might also be interested in it. Digi is offering a iMX53 Jumpstart Kit (CC-WMX53-ANDRD) for Android for $199.&amp;nbsp; It is a complete kit and includes a nice 7" LCD (with touch).&amp;nbsp; Here are some details:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;ConnectCore Wi-i.MX53 module&lt;BR /&gt; - 1 GHz i.MX53, 512 MB NAND Flash, 512 MB DDR2, -20 to +70° C&lt;/LI&gt;&lt;LI&gt;7" WVGA LCD panel with touchscreen&lt;/LI&gt;&lt;LI&gt;Digi JumpStart Kit development board &lt;BR /&gt; 3 serial ports (1 x RS-232/422/485, 1 x RS-232 Tx/Rx, 1 x TTL), VGA, HDMI 1.3, Ethernet (RJ-45), WLAN antenna connectors, SD/MMC slot, MicroSD slot, USB OTG, 4 x USB Host, I2C/SPI headers, 1-Wire connector, audio: line in/out and microphone in (3.5 mm), Digi XBee module socket module sold separately), GPIO screw terminal, user push-buttons, user LEDs, battery, 802.3af (PoE) module socket (module sold separately), external LCD/Touchscreen connectors, external camera connectors, user/application connectors, JTAG connector, 9-30VDC power supply, power switch&lt;/LI&gt;&lt;LI&gt;Power supply and accessories&lt;BR /&gt; - External wall power supply with adapters,&lt;BR /&gt; Ethernet cable, antennas, serial cable&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I just received mine yesterday and so I have not had too much time to play with it, other than just turning it on... it looks like I will be busy this weekend..&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Cheers,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;Sam&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Oct 2012 14:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221499#M14657</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2012-10-20T14:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: Excellent Dev Kit Deal for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221500#M14658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for sharing the information. Hope you have a great fun to play with the i.MX53 board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 08:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221500#M14658</guid>
      <dc:creator>JasonLiu</dc:creator>
      <dc:date>2012-10-22T08:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: Excellent Dev Kit Deal for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221501#M14659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day Hui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response!&amp;nbsp; Indeed, it is my pleasure to pass along pertinent info to all those that are interested.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the dev kit, sadly, I got sidetracked last weekend and so I was unable to work with the kit.&amp;nbsp; Hopefully things will free up a bit so that I can experiment with it further.&amp;nbsp; What I can say is that it is a very well designed kit and the screen is excellent and very responsive.&amp;nbsp; The Digi modules are indeed impressive and they do offer a variety to suit one's needs (i.e. some include Wifi, etc) and cost.&amp;nbsp; That being said, I do find the modules a bit pricey for use in our company's products.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2012 14:50:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Excellent-Dev-Kit-Deal-for-iMX53/m-p/221501#M14659</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2012-10-25T14:50:58Z</dc:date>
    </item>
  </channel>
</rss>