<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx8 USB DRD as USB3.0 SS Host  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-USB-DRD-as-USB3-0-SS-Host/m-p/985101#M146329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an issue regarding USB connectivity for the i.mx8 Soc:&lt;/P&gt;&lt;P&gt;The hardware has 2 usb components inside: one host and the other one is usb dual role capable.&lt;/P&gt;&lt;P&gt;I have the dual role instance configured for host mode, but I can't enumerate devices in superspeed - highspeed works well.&lt;/P&gt;&lt;P&gt;The device (in my case a hub) is connected using a special cable with a micro-a-plug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the Nitrogen8M hardware with ubuntu linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How is the procedure to get USB SS devices working on that USB instance?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Nov 2019 09:43:27 GMT</pubDate>
    <dc:creator>ralf_oberlaende</dc:creator>
    <dc:date>2019-11-28T09:43:27Z</dc:date>
    <item>
      <title>i.mx8 USB DRD as USB3.0 SS Host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8-USB-DRD-as-USB3-0-SS-Host/m-p/985101#M146329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an issue regarding USB connectivity for the i.mx8 Soc:&lt;/P&gt;&lt;P&gt;The hardware has 2 usb components inside: one host and the other one is usb dual role capable.&lt;/P&gt;&lt;P&gt;I have the dual role instance configured for host mode, but I can't enumerate devices in superspeed - highspeed works well.&lt;/P&gt;&lt;P&gt;The device (in my case a hub) is connected using a special cable with a micro-a-plug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the Nitrogen8M hardware with ubuntu linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How is the procedure to get USB SS devices working on that USB instance?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2019 09:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8-USB-DRD-as-USB3-0-SS-Host/m-p/985101#M146329</guid>
      <dc:creator>ralf_oberlaende</dc:creator>
      <dc:date>2019-11-28T09:43:27Z</dc:date>
    </item>
  </channel>
</rss>