<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Yocto Task #1 - Download the source code ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Task-1-Download-the-source-code/m-p/985069#M146324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To create embedded Linux image for imx8qxpmek evaluation board, I went to Yocto Training - Home as follows:&lt;/P&gt;&lt;P&gt;&lt;IMG /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started with Task #1 - Download the source code.&amp;nbsp; I was expecting that Task #1 would contain command to Download poky source:&amp;nbsp; $ git clone git://git.yoctoproject.org/poky --branch warrior&lt;/P&gt;&lt;P&gt;And then I thought Task #1 would provide following command to prepare the build:&lt;/P&gt;&lt;P&gt;$ source oe-init-build-en &amp;lt;build_directory&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But Task #1 is providing commands to download BSP source.&amp;nbsp; For which board are we downloading the BSP source?&lt;/P&gt;&lt;P&gt;Why is Task #1 asking to Download source code from community and NXP Code Aurora?&amp;nbsp; Shouldn't it be one or the other?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to Download poky source code using the git command above?&amp;nbsp; Or I'll get every needed to build yocto using commands in Task #1 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Dec 2019 19:05:53 GMT</pubDate>
    <dc:creator>anaseem</dc:creator>
    <dc:date>2019-12-16T19:05:53Z</dc:date>
    <item>
      <title>Yocto Task #1 - Download the source code ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Task-1-Download-the-source-code/m-p/985069#M146324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To create embedded Linux image for imx8qxpmek evaluation board, I went to Yocto Training - Home as follows:&lt;/P&gt;&lt;P&gt;&lt;IMG /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started with Task #1 - Download the source code.&amp;nbsp; I was expecting that Task #1 would contain command to Download poky source:&amp;nbsp; $ git clone git://git.yoctoproject.org/poky --branch warrior&lt;/P&gt;&lt;P&gt;And then I thought Task #1 would provide following command to prepare the build:&lt;/P&gt;&lt;P&gt;$ source oe-init-build-en &amp;lt;build_directory&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But Task #1 is providing commands to download BSP source.&amp;nbsp; For which board are we downloading the BSP source?&lt;/P&gt;&lt;P&gt;Why is Task #1 asking to Download source code from community and NXP Code Aurora?&amp;nbsp; Shouldn't it be one or the other?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to Download poky source code using the git command above?&amp;nbsp; Or I'll get every needed to build yocto using commands in Task #1 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 19:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Task-1-Download-the-source-code/m-p/985069#M146324</guid>
      <dc:creator>anaseem</dc:creator>
      <dc:date>2019-12-16T19:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Task #1 - Download the source code ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Task-1-Download-the-source-code/m-p/985070#M146325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Amer Naseem,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The Yocto training you are referencing to is focused on the Community BSP (more information on the link below)&lt;BR /&gt;&lt;A href="https://freescale.github.io/#documentation"&gt;https://freescale.github.io/#documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If you are working with an NXP board I would recommend starting with one of the BSP Releases, available at the following link:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?&amp;amp;tab=Documentation_Tab"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For the imx8qxpmek board the latest BSP Release available is L4.19.35_1.1.0. You can download the documentation for this BSP on the link below (you may need to login to download this documentation bundle)&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_LINUX_DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_LINUX_DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Inside, you will find the i.MX Yocto Project User's Guide, which has instructions on how to setup Yocto on your host machine to build images for this board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 15:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Task-1-Download-the-source-code/m-p/985070#M146325</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-12-20T15:08:54Z</dc:date>
    </item>
  </channel>
</rss>