<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How to Read the CPU Core Clock Frequency from dts file</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984805#M146295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sreedhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Karan Gajjar mentioned, you may read the actual CPU frequency from the cpufreq driver. You can find more details on how it works in the i.MX Linux Reference Manual available as part of the BSP documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the device tree frequency definitions, you are correct in that those would be theoretical and if could be that the frequencies listed are not achievable so you would need test them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jan 2020 15:03:01 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-01-16T15:03:01Z</dc:date>
    <item>
      <title>How to Read the CPU Core Clock Frequency from dts file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984803#M146293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with IMX8M Mini EVK Yocto Linux 4.14.98.2.0.0 version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can read the cpu current frequency from sys interface.&lt;/P&gt;&lt;P&gt;For example: I want to read the CPU0&lt;/P&gt;&lt;P&gt;cd /sys/devices/system/cpu/cpu0/cpufreq/&lt;/P&gt;&lt;P&gt;cat cpuinfo_cur_freq&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gives the current cpu frequency, is there any other way to find the cpu frequency apart from this.&lt;/P&gt;&lt;P&gt;from dts file can we read the value theoretically&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, Sreedhar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2020 15:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984803#M146293</guid>
      <dc:creator>sreedhar_appala</dc:creator>
      <dc:date>2020-01-08T15:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to Read the CPU Core Clock Frequency from dts file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984804#M146294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-userid="348707" data-username="sreedhar.appalayagari@sony.com" href="https://community.nxp.com/people/sreedhar.appalayagari@sony.com"&gt;Sreedhar A&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For finding CPU frequency you can used &lt;STRONG&gt;cpufreq-info&lt;/STRONG&gt; command it displays the current CPU frequency.In dts file there is CPU frequency operating points are available and due to the frequency scaling the current CPU frequency may vary within MIN and MAX operating points.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let us know in case of any concern&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karan Gajjar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2020 06:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984804#M146294</guid>
      <dc:creator>karangajjar</dc:creator>
      <dc:date>2020-01-10T06:26:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to Read the CPU Core Clock Frequency from dts file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984805#M146295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sreedhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Karan Gajjar mentioned, you may read the actual CPU frequency from the cpufreq driver. You can find more details on how it works in the i.MX Linux Reference Manual available as part of the BSP documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the device tree frequency definitions, you are correct in that those would be theoretical and if could be that the frequencies listed are not achievable so you would need test them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 15:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Read-the-CPU-Core-Clock-Frequency-from-dts-file/m-p/984805#M146295</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-01-16T15:03:01Z</dc:date>
    </item>
  </channel>
</rss>