<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Custom imx8mm DDR3</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-imx8mm-DDR3/m-p/984598#M146266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;The boot procedure of the i.MX8M includes loading&amp;nbsp; HDMI and DDR controller’s&amp;nbsp; firmware,&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;that must be loaded prior to executing the bootloader. Then - ATF should be run, and after that&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;U-boot starts. So, in U-boot , under A53 core, PMIC configuration may be&amp;nbsp; implemented.&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp; Use section 3.2.3 (Adding new driver initialization code to board files) of Chapter 3&amp;nbsp; (Porting &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;U-Boot) of “i.MX_Porting_Guide.pdf”.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Nov 2019 06:06:07 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2019-11-14T06:06:07Z</dc:date>
    <item>
      <title>Custom imx8mm DDR3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-imx8mm-DDR3/m-p/984597#M146265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We know that &lt;STRONG&gt;iMX8MM&lt;/STRONG&gt; boards use low power &lt;STRONG&gt;DDR4&lt;/STRONG&gt; and getting &lt;STRONG&gt;1.1V&lt;/STRONG&gt; from &lt;STRONG&gt;PMIC&lt;/STRONG&gt; while running up the board,&lt;/P&gt;&lt;P&gt;But we made our custom board based on the same &lt;STRONG&gt;iMX8MM&lt;/STRONG&gt; architecture but we chose to use &lt;STRONG&gt;DDR3&lt;/STRONG&gt; instead, and for that reason the tension for the &lt;STRONG&gt;BUCK8&lt;/STRONG&gt; register of the &lt;STRONG&gt;Cortex&lt;/STRONG&gt;-&lt;STRONG&gt;m4&lt;/STRONG&gt; need to get &lt;STRONG&gt;1.35V&lt;/STRONG&gt; as showing this table:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot from 2019-11-13 10-48-16.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92538i6ED317D5397C448C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2019-11-13 10-48-16.png" alt="Screenshot from 2019-11-13 10-48-16.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In order to achieve that, we made these steps:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&amp;nbsp;Connect &lt;STRONG&gt;JLINK EDU version10.1&lt;/STRONG&gt; with the &lt;STRONG&gt;iMX8MM&lt;/STRONG&gt; &lt;STRONG&gt;JTAG&lt;/STRONG&gt; pins&lt;/LI&gt;&lt;LI&gt;Use &lt;STRONG&gt;IAR&lt;/STRONG&gt; embedded software with &lt;STRONG&gt;iMX8mm&lt;/STRONG&gt; patch to connect with the &lt;STRONG&gt;Cortex-m4&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Connection is successfully achieved&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Now when we make simple LED blinking test example it works fine, but after rebooting the board the program is gone,&lt;/P&gt;&lt;P&gt;so it's programmed in the RAM and we don't know where/how to make it permanent,&lt;/P&gt;&lt;P&gt;we did check that the &lt;STRONG&gt;Cortex-m4&lt;/STRONG&gt; of &lt;STRONG&gt;IMX8MM&lt;/STRONG&gt; has no flash size.&lt;/P&gt;&lt;P&gt;So the question is: where and how to change the &lt;STRONG&gt;BUCK8&lt;/STRONG&gt; register and make that permanent so our &lt;STRONG&gt;DDR3 RAM&lt;/STRONG&gt; be loaded in order to boot the eMMC/sdcard Linux image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" data-type="grammar" title="Please add a punctuation mark at the end of paragraph"&gt;Best regards,&lt;BR /&gt; Houssem&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 10:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-imx8mm-DDR3/m-p/984597#M146265</guid>
      <dc:creator>houssem_chaaban</dc:creator>
      <dc:date>2019-11-13T10:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: Custom imx8mm DDR3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-imx8mm-DDR3/m-p/984598#M146266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;The boot procedure of the i.MX8M includes loading&amp;nbsp; HDMI and DDR controller’s&amp;nbsp; firmware,&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;that must be loaded prior to executing the bootloader. Then - ATF should be run, and after that&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;U-boot starts. So, in U-boot , under A53 core, PMIC configuration may be&amp;nbsp; implemented.&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp; Use section 3.2.3 (Adding new driver initialization code to board files) of Chapter 3&amp;nbsp; (Porting &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;U-Boot) of “i.MX_Porting_Guide.pdf”.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Nov 2019 06:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-imx8mm-DDR3/m-p/984598#M146266</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-11-14T06:06:07Z</dc:date>
    </item>
  </channel>
</rss>