<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX8M Core Temperature Problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Core-Temperature-Problem/m-p/984046#M146200</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;We are using IMX8M (Version 1.2) running over our own test board (size and structure similar to EVK board) and we made a temperature test by checking the&amp;nbsp;/sys/class/thermal/thermal_zone0/temp for reading out the core temperature &lt;STRONG&gt;without cooling unit.&amp;nbsp;&lt;/STRONG&gt;Ambient temperature was the same for all tests. All other configs including modules loaded are the same.&lt;/P&gt;&lt;P&gt;We have the following results:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;&amp;gt;Yocto Sumo 4.14.78 (built Linux from source code) runs for 30 mins and then shuts down at 76 degrees.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;gt;&amp;gt;&lt;SPAN&gt;Yocto Sumo 4.14.78 (built Linux using bitbake, base_image), which runs continuously at 67&amp;nbsp;degrees without shutting down even after 1 hour.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;gt;&amp;gt;Yocto Morty&lt;SPAN&gt;&amp;nbsp;(built Linux from source code)&amp;nbsp;&lt;/SPAN&gt;keeps running at 70 degrees without shutting down even after 1 hour.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please share any information or related documents that can help us understand why there is a difference between when we use bitbake Vs built from source code for Sumo with respect to the core temperature?&amp;nbsp; Even when the board has a tolerance of higher core temperature why does it shut down?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Mar 2020 10:45:54 GMT</pubDate>
    <dc:creator>joachimjaehn</dc:creator>
    <dc:date>2020-03-04T10:45:54Z</dc:date>
    <item>
      <title>IMX8M Core Temperature Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Core-Temperature-Problem/m-p/984046#M146200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;We are using IMX8M (Version 1.2) running over our own test board (size and structure similar to EVK board) and we made a temperature test by checking the&amp;nbsp;/sys/class/thermal/thermal_zone0/temp for reading out the core temperature &lt;STRONG&gt;without cooling unit.&amp;nbsp;&lt;/STRONG&gt;Ambient temperature was the same for all tests. All other configs including modules loaded are the same.&lt;/P&gt;&lt;P&gt;We have the following results:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;&amp;gt;Yocto Sumo 4.14.78 (built Linux from source code) runs for 30 mins and then shuts down at 76 degrees.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;gt;&amp;gt;&lt;SPAN&gt;Yocto Sumo 4.14.78 (built Linux using bitbake, base_image), which runs continuously at 67&amp;nbsp;degrees without shutting down even after 1 hour.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;gt;&amp;gt;Yocto Morty&lt;SPAN&gt;&amp;nbsp;(built Linux from source code)&amp;nbsp;&lt;/SPAN&gt;keeps running at 70 degrees without shutting down even after 1 hour.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please share any information or related documents that can help us understand why there is a difference between when we use bitbake Vs built from source code for Sumo with respect to the core temperature?&amp;nbsp; Even when the board has a tolerance of higher core temperature why does it shut down?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2020 10:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Core-Temperature-Problem/m-p/984046#M146200</guid>
      <dc:creator>joachimjaehn</dc:creator>
      <dc:date>2020-03-04T10:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Core Temperature Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Core-Temperature-Problem/m-p/984047#M146201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="302116" data-username="joachimjaehn" href="https://community.nxp.com/people/joachimjaehn"&gt;joachim &lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. &lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;We don't have the documentation you want.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. &lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;About core temperature monitoring&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;There is a thermal driver in the Linux BSP. The file name is drivers / thermal / imx_thermal.c. You can adjust the shutdown temperature.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;Hope above infromation is helpful for you!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;Have a nice day!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;B.R,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;Weidong&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2020 05:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Core-Temperature-Problem/m-p/984047#M146201</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-03-17T05:24:58Z</dc:date>
    </item>
  </channel>
</rss>