<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX53 and SPDIF input</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221112#M14591</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can anybody know, what kind of input is SPDIF_Rx pin? Do i need to transform tipical SPDIF signal to TLL logic [3.3V] or is it this transformation done in processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrej Barbis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Oct 2012 05:30:55 GMT</pubDate>
    <dc:creator>AndrejBarbis</dc:creator>
    <dc:date>2012-10-19T05:30:55Z</dc:date>
    <item>
      <title>iMX53 and SPDIF input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221112#M14591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can anybody know, what kind of input is SPDIF_Rx pin? Do i need to transform tipical SPDIF signal to TLL logic [3.3V] or is it this transformation done in processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrej Barbis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2012 05:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221112#M14591</guid>
      <dc:creator>AndrejBarbis</dc:creator>
      <dc:date>2012-10-19T05:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 and SPDIF input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221113#M14592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The (input) signals&amp;nbsp; should be transformed to voltage level NVCC_GPIO. &lt;BR /&gt;There are three working points for NVCC_GPIO : 1.8V ; 2.775V ; 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;High-Level DC input voltage,VIH&amp;nbsp; should be in range 0.7V x NVCC_GPIO - NVCC_GPIO.&lt;/P&gt;&lt;P&gt;Low-Level DC input voltage, VIL should be in range 0V&amp;nbsp; - 0.3 x NVCC_GPIO.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 08:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221113#M14592</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2012-10-24T08:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 and SPDIF input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221114#M14593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrej and Yuri,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;One thing to be care ful of. SPDIF or IEC60958 signal is 0.5 to 0.6V Pk-pk.&amp;nbsp; So, yes you have to convert the signal level of your choice to match what Yuri mentioned.&amp;nbsp; One other thing to be really careful is to make sure that the edge rate and propagation delay for rise/fall time must be kept or you will end up with severe jitter degrading the signal quality.&amp;nbsp; So, make sure to use high speed level shifter with close rise/fall time spec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, depending on whether Coax (75ohm) or Optical connection could change the signal level, too.&amp;nbsp; So you may have to factor that in. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Take care.&lt;/P&gt;&lt;P&gt;Haku&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 12:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-and-SPDIF-input/m-p/221114#M14593</guid>
      <dc:creator>haku_sato</dc:creator>
      <dc:date>2012-10-26T12:46:54Z</dc:date>
    </item>
  </channel>
</rss>