<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWhat happens for the Yocto Linux rootfs size?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981688#M145851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using IMX8mini EVK, which is 8G emmc, running Yocto Linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default, the bitbake fsl-image-validation-imx would created a 1.3GB size of rootfs, like&amp;nbsp;fsl-image-validation-imx-imx8mmevk.sdcard.bz2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After flashing the whole image, the linux would show the rootfs(/) is the same size as 1.3GB. But we all know our emmc is 8GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I struggling this, found if add IMAGE_ROOTFS_SIZE with large number to increase the whole size.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviouslly, this is un-reasonable, as we have to create 8GB file size of rootfs image, that's too large for both flash and copying. I am really feel confused that why Yocto Linux use such method? As most of the data byte must be ZERO-padding for this case, this is unnecessary at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Android, the whole system.img is just 800MB, but the whole 8GB emmc can be usable and visable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How could I let Yocto Linux have real data size(e.g, just 400MB), but the whole emmc storage also be visable and usable?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 09:26:44 GMT</pubDate>
    <dc:creator>13614278</dc:creator>
    <dc:date>2020-03-18T09:26:44Z</dc:date>
    <item>
      <title>What happens for the Yocto Linux rootfs size?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981688#M145851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using IMX8mini EVK, which is 8G emmc, running Yocto Linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default, the bitbake fsl-image-validation-imx would created a 1.3GB size of rootfs, like&amp;nbsp;fsl-image-validation-imx-imx8mmevk.sdcard.bz2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After flashing the whole image, the linux would show the rootfs(/) is the same size as 1.3GB. But we all know our emmc is 8GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I struggling this, found if add IMAGE_ROOTFS_SIZE with large number to increase the whole size.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviouslly, this is un-reasonable, as we have to create 8GB file size of rootfs image, that's too large for both flash and copying. I am really feel confused that why Yocto Linux use such method? As most of the data byte must be ZERO-padding for this case, this is unnecessary at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Android, the whole system.img is just 800MB, but the whole 8GB emmc can be usable and visable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How could I let Yocto Linux have real data size(e.g, just 400MB), but the whole emmc storage also be visable and usable?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 09:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981688#M145851</guid>
      <dc:creator>13614278</dc:creator>
      <dc:date>2020-03-18T09:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: What happens for the Yocto Linux rootfs size?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981689#M145852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yang Songxiang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I agree that it’s hard to fir the resulting image to your storage size. The following document may be helpful:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105521"&gt;https://community.nxp.com/docs/DOC-105521&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend increasing the free space (IMAGE_ROOTFS_EXTRA_SPACE), which is an easier parameter to setup in order to maximize the use of the storage used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 18:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981689#M145852</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-03-18T18:35:11Z</dc:date>
    </item>
    <item>
      <title>Re: What happens for the Yocto Linux rootfs size?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981690#M145853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much, this is the first time that I got my expected answer on this website.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 03:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-happens-for-the-Yocto-Linux-rootfs-size/m-p/981690#M145853</guid>
      <dc:creator>13614278</dc:creator>
      <dc:date>2020-03-19T03:38:07Z</dc:date>
    </item>
  </channel>
</rss>