<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to check Cable diagnostics for TJA1100 PHY  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980113#M145701</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We are using the TJA1100 as a PHY with MPC5746C.&lt;BR /&gt;I need to check the cable errors during the run time, either for open/short circuit between the twisted pair cables.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;So I actually tried to shorten the two wires or unplug the cable from the Trcv connector and indeed I got the Link-fail counter interrupt which is fired due to the high losses/noisy channel and inside this interrupt ISR I'm gonna run the cable diagnostics, But I have some inquires &lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;1 - If an open or short circuit happened, shall this forces the Trcv chip to go to Power down mode or it will stay in the power up mode ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;2 - Is there a specific procedure to check the cable errors " shall I write some bits in any registers " ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;according to the cabling errors section, shall I put the controller in power down mode to disable all communications ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;and then set the cable test bit, then reset the Trcv in power up as it was ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Cabling errors.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92043iD18E4A42A9F479BA/image-size/large?v=v2&amp;amp;px=999" role="button" title="Cabling errors.PNG" alt="Cabling errors.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;3 - I have a very weird observation: while the controller is communicating by debugging I found that the POWER_DOWN bit in the Basic control register (Register 0) equals 1, and as stated in the datasheet 1 means Trcv is in power down.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;meanwhile the POWER_MODE bits(14:11) in the Extended control register (Register 17) give the value 0011 which means normal mode, so what is wrong here ? &lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Power down.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92008i16F98E50C42D0E97/image-size/large?v=v2&amp;amp;px=999" role="button" title="Power down.PNG" alt="Power down.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;4 - Also when I shorten the two twisted wires or unplugged them and read the&amp;nbsp;External status register (Register 25)&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;and check on bit 7&amp;amp;8, I found that it didn't indicate any problem, I mean it is saying that there is no cable errors while I'm forcing a shorten or opening to the wires.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thanks&lt;BR /&gt;Ahmed Saber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Oct 2019 21:05:52 GMT</pubDate>
    <dc:creator>ahmedsaber</dc:creator>
    <dc:date>2019-10-29T21:05:52Z</dc:date>
    <item>
      <title>How to check Cable diagnostics for TJA1100 PHY</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980113#M145701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We are using the TJA1100 as a PHY with MPC5746C.&lt;BR /&gt;I need to check the cable errors during the run time, either for open/short circuit between the twisted pair cables.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;So I actually tried to shorten the two wires or unplug the cable from the Trcv connector and indeed I got the Link-fail counter interrupt which is fired due to the high losses/noisy channel and inside this interrupt ISR I'm gonna run the cable diagnostics, But I have some inquires &lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;1 - If an open or short circuit happened, shall this forces the Trcv chip to go to Power down mode or it will stay in the power up mode ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;2 - Is there a specific procedure to check the cable errors " shall I write some bits in any registers " ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;according to the cabling errors section, shall I put the controller in power down mode to disable all communications ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;and then set the cable test bit, then reset the Trcv in power up as it was ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Cabling errors.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92043iD18E4A42A9F479BA/image-size/large?v=v2&amp;amp;px=999" role="button" title="Cabling errors.PNG" alt="Cabling errors.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;3 - I have a very weird observation: while the controller is communicating by debugging I found that the POWER_DOWN bit in the Basic control register (Register 0) equals 1, and as stated in the datasheet 1 means Trcv is in power down.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;meanwhile the POWER_MODE bits(14:11) in the Extended control register (Register 17) give the value 0011 which means normal mode, so what is wrong here ? &lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Power down.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92008i16F98E50C42D0E97/image-size/large?v=v2&amp;amp;px=999" role="button" title="Power down.PNG" alt="Power down.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;4 - Also when I shorten the two twisted wires or unplugged them and read the&amp;nbsp;External status register (Register 25)&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;and check on bit 7&amp;amp;8, I found that it didn't indicate any problem, I mean it is saying that there is no cable errors while I'm forcing a shorten or opening to the wires.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thanks&lt;BR /&gt;Ahmed Saber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 21:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980113#M145701</guid>
      <dc:creator>ahmedsaber</dc:creator>
      <dc:date>2019-10-29T21:05:52Z</dc:date>
    </item>
    <item>
      <title>Re: How to check Cable diagnostics for TJA1100 PHY</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980114#M145702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You cannot get cable errors during the normal operation, you can only&lt;BR /&gt;see the link status change. Cable errors are result of cable diagnostics &lt;BR /&gt;which is _not_ the normal mode and requires LINK_CONTROL = 0. &lt;BR /&gt;Refer to AN12088 Section 5.2.2 for Link Status,&lt;BR /&gt;to Section 6.1 for the function of LINK_CONTROL and to Sections 6.4&lt;BR /&gt;and 6.5 for test modes. The document can be found on the public&lt;BR /&gt;SJA1100 Product Page:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12088.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12088.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2019 18:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980114#M145702</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2019-11-01T18:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to check Cable diagnostics for TJA1100 PHY</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980115#M145703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello bpe,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt;As mentioned in the application note: &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;SPAN class=""&gt;6.5 Cable test&lt;/SPAN&gt; &lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Cable test trigger.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92055i8511FF1939272A7F/image-size/large?v=v2&amp;amp;px=999" role="button" title="Cable test trigger.PNG" alt="Cable test trigger.PNG" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;SPAN class=""&gt;6.1 Link control&lt;/SPAN&gt; &lt;BR style="font-style: normal; font-variant: normal; font-weight: normal; letter-spacing: normal; line-height: normal; orphans: 2; text-align: -webkit-auto; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-size-adjust: auto; -webkit-text-stroke-width: 0px;" /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Link Control.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92098i835CE85F1B724533/image-size/large?v=v2&amp;amp;px=999" role="button" title="Link Control.PNG" alt="Link Control.PNG" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; So I'm little confused, how PHY must be in normal mode and required to disable the link control, while disabling the link control will force a transition to standby mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt;then PHY is not in the normal mode yet.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt;Also: what about points 3 &amp;amp; 4 in the original question,&amp;nbsp; do you have any explanation or suggestion what is wrong ?&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt;Could you please clarify the answers for each questions in their positions &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Ahmed Saber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2019 19:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980115#M145703</guid>
      <dc:creator>ahmedsaber</dc:creator>
      <dc:date>2019-11-01T19:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to check Cable diagnostics for TJA1100 PHY</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980116#M145704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any response please&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Nov 2019 09:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-check-Cable-diagnostics-for-TJA1100-PHY/m-p/980116#M145704</guid>
      <dc:creator>ahmedsaber</dc:creator>
      <dc:date>2019-11-11T09:42:52Z</dc:date>
    </item>
  </channel>
</rss>