<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX6UL Mic. Recording Problem!! in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Mic-Recording-Problem/m-p/978874#M145602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMX6ULevk board with wm8960 codec&amp;nbsp; but im facing problem of mic recording.when i give arecord command it records the audio without throwing any error but when i aplay the mic recorded wav file there is no output.&lt;/P&gt;&lt;P&gt;But when i aplay the demo wav files there is output through speakers.&lt;/P&gt;&lt;P&gt;so please can i know which part of driver/dts i need to cross check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Dec 2019 10:47:31 GMT</pubDate>
    <dc:creator>dhanushvenugopa</dc:creator>
    <dc:date>2019-12-14T10:47:31Z</dc:date>
    <item>
      <title>I.MX6UL Mic. Recording Problem!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Mic-Recording-Problem/m-p/978874#M145602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMX6ULevk board with wm8960 codec&amp;nbsp; but im facing problem of mic recording.when i give arecord command it records the audio without throwing any error but when i aplay the mic recorded wav file there is no output.&lt;/P&gt;&lt;P&gt;But when i aplay the demo wav files there is output through speakers.&lt;/P&gt;&lt;P&gt;so please can i know which part of driver/dts i need to cross check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Dec 2019 10:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Mic-Recording-Problem/m-p/978874#M145602</guid>
      <dc:creator>dhanushvenugopa</dc:creator>
      <dc:date>2019-12-14T10:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6UL Mic. Recording Problem!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Mic-Recording-Problem/m-p/978875#M145603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;Dhanush&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check registered audio devices using sect.7.1.2.4 Sound Card Information and some&lt;/P&gt;&lt;P&gt;alsa methods described in sect.7.4.3 attached Linux Manual.&lt;/P&gt;&lt;P&gt;Please try with &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_MX6UL7D&amp;amp;appType=license" target="_blank"&gt;Linux Binary Demo Files - i.MX 6UltraLite, i.MX 6ULL, i.MX 7Dual&lt;/A&gt;&lt;/P&gt;&lt;P&gt;May be useful some audio unit tests:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_amix_test?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_amix_test?h=imx_4.14.78_1.0.0_ga"&gt;mxc_amix_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 23:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Mic-Recording-Problem/m-p/978875#M145603</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-12-16T23:51:31Z</dc:date>
    </item>
  </channel>
</rss>