<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Boot_cfg fuse issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-cfg-fuse-issue/m-p/975471#M145186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the rt1050 evkb, I need to check something about the Boot CFG[0:11], When Boot CFG[0:11] set up, The FDCB of the Boot image is error value, Can used the "NXP Boot Utility" rebuild or erase flash (Boot Mode= 0'b01) ?&lt;/P&gt;&lt;P&gt;I think it can, but I need a definitive answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to directed against sample code of burning&amp;nbsp;&lt;SPAN style="color: #3d3d3d; "&gt;boot cfg[0:11] fused to reference,&amp;nbsp;because I'm not sure, Is the program I wrote correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regard&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Dec 2019 07:38:27 GMT</pubDate>
    <dc:creator>jimhuang2</dc:creator>
    <dc:date>2019-12-13T07:38:27Z</dc:date>
    <item>
      <title>Boot_cfg fuse issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-cfg-fuse-issue/m-p/975471#M145186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the rt1050 evkb, I need to check something about the Boot CFG[0:11], When Boot CFG[0:11] set up, The FDCB of the Boot image is error value, Can used the "NXP Boot Utility" rebuild or erase flash (Boot Mode= 0'b01) ?&lt;/P&gt;&lt;P&gt;I think it can, but I need a definitive answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to directed against sample code of burning&amp;nbsp;&lt;SPAN style="color: #3d3d3d; "&gt;boot cfg[0:11] fused to reference,&amp;nbsp;because I'm not sure, Is the program I wrote correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regard&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 07:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-cfg-fuse-issue/m-p/975471#M145186</guid>
      <dc:creator>jimhuang2</dc:creator>
      <dc:date>2019-12-13T07:38:27Z</dc:date>
    </item>
    <item>
      <title>Re: Boot_cfg fuse issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-cfg-fuse-issue/m-p/975472#M145187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="322065" data-username="jimhuang@alltekmarine.com" href="https://community.nxp.com/people/jimhuang@alltekmarine.com"&gt;JingHuan Huang&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Can I use the "NXP Boot Utility" rebuild or erase the flash (Boot Mode= 0'b01)?&lt;BR /&gt;-- Yes, the NXP Boot Utility is able to erase the flash and burn the fuse map.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 01:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-cfg-fuse-issue/m-p/975472#M145187</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-12-16T01:56:39Z</dc:date>
    </item>
  </channel>
</rss>