<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6 GPIO current sinking capability</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-current-sinking-capability/m-p/974860#M145114</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am designing a board which uses the IMX6ULL. I have a GPIO pin from the IMX6ULL controlling the reset pin for a module SOC on my board. The reset pin is active high. I would like to be able to manually put the module into reset during development. If the GPIO from the IMX6 (say GPIO_IO5) is driving the module reset pin low, and I force the reset high (like shorting a test point on reset to VCC_3V3) would this cause any issues with the GPIO?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jan 2020 22:52:05 GMT</pubDate>
    <dc:creator>adomino</dc:creator>
    <dc:date>2020-01-17T22:52:05Z</dc:date>
    <item>
      <title>IMX6 GPIO current sinking capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-current-sinking-capability/m-p/974860#M145114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am designing a board which uses the IMX6ULL. I have a GPIO pin from the IMX6ULL controlling the reset pin for a module SOC on my board. The reset pin is active high. I would like to be able to manually put the module into reset during development. If the GPIO from the IMX6 (say GPIO_IO5) is driving the module reset pin low, and I force the reset high (like shorting a test point on reset to VCC_3V3) would this cause any issues with the GPIO?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 22:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-current-sinking-capability/m-p/974860#M145114</guid>
      <dc:creator>adomino</dc:creator>
      <dc:date>2020-01-17T22:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 GPIO current sinking capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-current-sinking-capability/m-p/974861#M145115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;would this cause any issues with the GPIO?&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, it wouldn't.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Generally speaking, the limitation of PIN's sink current should be less than 17.8mA.&lt;/P&gt;&lt;P&gt;So you should pay attention to controlling sink current.&lt;/P&gt;&lt;P&gt;If the sink current is too large, it is easy to cause internal circuit leakage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jan 2020 06:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-current-sinking-capability/m-p/974861#M145115</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-01-19T06:30:19Z</dc:date>
    </item>
  </channel>
</rss>