<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 About Power mode transitions</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-Power-mode-transitions/m-p/974319#M145010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two questions about Table 6-8 Power mode transitions in i.MX 7 Dual Applications Processor Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) Does this mean that timer interrupt is enabled by LP Time Alarm Enable in SNVS_LP Control Register (LPCR)?&lt;BR /&gt;Which field should I check to see if an interrupt was asserted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2)&amp;nbsp;If DP_EN of SNVS_LP Control Register (LPCR), can PMIC_ON_REQ signal be set to 0 in TOP?&lt;/P&gt;&lt;P&gt;Table 6-8. Is the Configuration with internal PMIC column of Power mode transitions Dumb PMIC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best reguards&lt;/P&gt;&lt;P&gt;Goto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Aug 2019 05:24:01 GMT</pubDate>
    <dc:creator>goto11</dc:creator>
    <dc:date>2019-08-27T05:24:01Z</dc:date>
    <item>
      <title>About Power mode transitions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-Power-mode-transitions/m-p/974319#M145010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two questions about Table 6-8 Power mode transitions in i.MX 7 Dual Applications Processor Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) Does this mean that timer interrupt is enabled by LP Time Alarm Enable in SNVS_LP Control Register (LPCR)?&lt;BR /&gt;Which field should I check to see if an interrupt was asserted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2)&amp;nbsp;If DP_EN of SNVS_LP Control Register (LPCR), can PMIC_ON_REQ signal be set to 0 in TOP?&lt;/P&gt;&lt;P&gt;Table 6-8. Is the Configuration with internal PMIC column of Power mode transitions Dumb PMIC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best reguards&lt;/P&gt;&lt;P&gt;Goto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 05:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-Power-mode-transitions/m-p/974319#M145010</guid>
      <dc:creator>goto11</dc:creator>
      <dc:date>2019-08-27T05:24:01Z</dc:date>
    </item>
    <item>
      <title>Re: About Power mode transitions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-Power-mode-transitions/m-p/974320#M145011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GoTo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. yes. It can be checked using SNVS_LPSR bit LPTA&lt;/P&gt;&lt;P&gt;2. yes it is dumb mode, usage TOP and DP_EN can be found in patch on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-339779"&gt;Q&amp;amp;amp;A: How is mx6 PMIC_ON_REQ under SW control?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 09:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-Power-mode-transitions/m-p/974320#M145011</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-27T09:37:11Z</dc:date>
    </item>
  </channel>
</rss>