<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: MCIMX8QuadMax Boot-UP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8QuadMax-Boot-UP/m-p/973660#M144923</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can try to refer to this &lt;A href="https://community.nxp.com/docs/DOC-342719"&gt;https://community.nxp.com/docs/DOC-342719&lt;/A&gt; , install the usb driver. If it does not work contact us.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jun 2019 09:58:21 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2019-06-28T09:58:21Z</dc:date>
    <item>
      <title>MCIMX8QuadMax Boot-UP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8QuadMax-Boot-UP/m-p/973659#M144922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I have&amp;nbsp;i.MX QuadMax MEK CPU board, of which the CM4 core I want to use for a bare metal application.&lt;/P&gt;&lt;P&gt;As instructed by the Quick Start Guide I received along with the board, placed&amp;nbsp;my image file in the SD Card and set the Bootmode switches to 001100 so that SDCard is used by the Boot-ROM for booting the system up.&lt;/P&gt;&lt;P&gt;The quick start guide also instructs to configure&amp;nbsp;a terminal window(Teraterm) with parameters&amp;nbsp;&lt;/P&gt;&lt;P&gt;Baudrate: 115200&lt;/P&gt;&lt;P&gt;Data bits: 8&lt;/P&gt;&lt;P&gt;Stop bit: 1&lt;/P&gt;&lt;P&gt;Parity: None&lt;/P&gt;&lt;P&gt;Flow Control: None&lt;/P&gt;&lt;P&gt;and connect the board to PC acting as host&amp;nbsp;in order to&amp;nbsp;monitor the boot activity on the terminal with a micro-usb cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It does not mention the VCP drivers to install and eventually, no COM ports for serial communication are available to be configured in the terminal window.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 4 unrecognized devices visible though under the "Other devices" section in Device Manager by the name of "USB Serial Port".&lt;/P&gt;&lt;P&gt;Could someone please point me in a direction where I can find the drivers for this specific target or a detailed Boot process?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx8quadmax‌imx8quadmax-boot‌imx8quadmax-drivers‌MCIMX8QM-CPU&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 12:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8QuadMax-Boot-UP/m-p/973659#M144922</guid>
      <dc:creator>mehran_ali</dc:creator>
      <dc:date>2019-06-26T12:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8QuadMax Boot-UP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8QuadMax-Boot-UP/m-p/973660#M144923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can try to refer to this &lt;A href="https://community.nxp.com/docs/DOC-342719"&gt;https://community.nxp.com/docs/DOC-342719&lt;/A&gt; , install the usb driver. If it does not work contact us.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 09:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8QuadMax-Boot-UP/m-p/973660#M144923</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-06-28T09:58:21Z</dc:date>
    </item>
  </channel>
</rss>