<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8QXP ADC1 Clock</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-ADC1-Clock/m-p/972585#M144791</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am using IMX8QXP in which i have configured ADC0 , but i have to configure ADC1 and read it ,problem is that there no clock entry for ADC1 ,And if try to use ADC0's clock then it shows following error.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;imx8qxp_adc 5a89000.adc: Could not prepare or enable the clock&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have done required changes in device tree, only problem&amp;nbsp; now is clock for ADC1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so can someone help me, what clock should i use for ADC1&lt;/P&gt;&lt;P&gt;Thanks in Advance&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Aug 2019 11:26:10 GMT</pubDate>
    <dc:creator>swapnil_ks</dc:creator>
    <dc:date>2019-08-26T11:26:10Z</dc:date>
    <item>
      <title>IMX8QXP ADC1 Clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-ADC1-Clock/m-p/972585#M144791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am using IMX8QXP in which i have configured ADC0 , but i have to configure ADC1 and read it ,problem is that there no clock entry for ADC1 ,And if try to use ADC0's clock then it shows following error.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;imx8qxp_adc 5a89000.adc: Could not prepare or enable the clock&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have done required changes in device tree, only problem&amp;nbsp; now is clock for ADC1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so can someone help me, what clock should i use for ADC1&lt;/P&gt;&lt;P&gt;Thanks in Advance&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 11:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-ADC1-Clock/m-p/972585#M144791</guid>
      <dc:creator>swapnil_ks</dc:creator>
      <dc:date>2019-08-26T11:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP ADC1 Clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-ADC1-Clock/m-p/972586#M144792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I’m afraid that i.MX8QXP family is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 17:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-ADC1-Clock/m-p/972586#M144792</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-08-26T17:51:32Z</dc:date>
    </item>
  </channel>
</rss>