<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NXP i.MX6ULL EVK and Linux Kernel CONFIG_SMP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX6ULL-EVK-and-Linux-Kernel-CONFIG-SMP/m-p/972324#M144782</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, for processor with one core linux CONFIG_SMP is not needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jul 2019 04:37:47 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-07-11T04:37:47Z</dc:date>
    <item>
      <title>NXP i.MX6ULL EVK and Linux Kernel CONFIG_SMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX6ULL-EVK-and-Linux-Kernel-CONFIG-SMP/m-p/972323#M144781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The default kernel configuration file for i.MX6ULL EVK has the CONFIG_SMP set.&lt;/P&gt;&lt;P&gt;I was wondering if the CONFIG_SMP should be set for uniprocessor systems like i.MX6ULL.&lt;/P&gt;&lt;P&gt;If so, what would be a use case or a reason for enabling CONFIG_SMP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding is that CONFIG_SMP should be unset for uniprocessor systems for efficiency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dawei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 23:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX6ULL-EVK-and-Linux-Kernel-CONFIG-SMP/m-p/972323#M144781</guid>
      <dc:creator>daweichen</dc:creator>
      <dc:date>2019-07-10T23:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: NXP i.MX6ULL EVK and Linux Kernel CONFIG_SMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX6ULL-EVK-and-Linux-Kernel-CONFIG-SMP/m-p/972324#M144782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, for processor with one core linux CONFIG_SMP is not needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2019 04:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX6ULL-EVK-and-Linux-Kernel-CONFIG-SMP/m-p/972324#M144782</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-11T04:37:47Z</dc:date>
    </item>
  </channel>
</rss>