<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx53 custom linux, recording HD video in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx53-custom-linux-recording-HD-video/m-p/220761#M14472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. We have created our own board based on SMD and LOCO and added camera ov5640.&lt;/P&gt;&lt;P&gt;I am using kernel &lt;A href="https://github.com/Freescale/linux-imx/tree/patches-imx-2.6.35_11.09.01"&gt;patches-imx-2.6.35_11.09.0 &lt;/A&gt;from github. Filesystem is Ubuntu armhf.&lt;/P&gt;&lt;P&gt;Camera driver is loaded with all dependencies and I can record videos with tools like avconv, ffmpeg. But everything hangs when using mencoder of gstreamer, and in kernel log I can see calling this all the time:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In MVC: mxc_v4l_do_ioctl c0485619&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_ENUMSTD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;What I really want is to get better video cam resolution and it doesn really get&amp;nbsp; better changing ffmpeg parameters. As I've seen others on IMX community use gstreamer, but I can't get it working with parameter "&lt;/SPAN&gt;mfw_v4lsrc&lt;SPAN class="mce_paste_marker"&gt;". &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Should I install Freescale provided .deb packages to get this working? But they all are armel, but I have armhf system.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I've tried to change capture mode in driver and it changes to 1280x720, but what is the v2f value, which still stays low? &lt;/SPAN&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; KERNEL LOG:&amp;nbsp; End of mxc_v4l_open: v2f pix widthxheight 288 x 352&lt;/P&gt;&lt;P&gt;Because it looks like ffmpeg is using this resolution.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jan 2013 15:21:55 GMT</pubDate>
    <dc:creator>janiscoders</dc:creator>
    <dc:date>2013-01-04T15:21:55Z</dc:date>
    <item>
      <title>imx53 custom linux, recording HD video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-custom-linux-recording-HD-video/m-p/220761#M14472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. We have created our own board based on SMD and LOCO and added camera ov5640.&lt;/P&gt;&lt;P&gt;I am using kernel &lt;A href="https://github.com/Freescale/linux-imx/tree/patches-imx-2.6.35_11.09.01"&gt;patches-imx-2.6.35_11.09.0 &lt;/A&gt;from github. Filesystem is Ubuntu armhf.&lt;/P&gt;&lt;P&gt;Camera driver is loaded with all dependencies and I can record videos with tools like avconv, ffmpeg. But everything hangs when using mencoder of gstreamer, and in kernel log I can see calling this all the time:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In MVC:mxc_v4l_ioctl&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In MVC: mxc_v4l_do_ioctl c0485619&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case VIDIOC_ENUMSTD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;What I really want is to get better video cam resolution and it doesn really get&amp;nbsp; better changing ffmpeg parameters. As I've seen others on IMX community use gstreamer, but I can't get it working with parameter "&lt;/SPAN&gt;mfw_v4lsrc&lt;SPAN class="mce_paste_marker"&gt;". &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Should I install Freescale provided .deb packages to get this working? But they all are armel, but I have armhf system.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;I've tried to change capture mode in driver and it changes to 1280x720, but what is the v2f value, which still stays low? &lt;/SPAN&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; KERNEL LOG:&amp;nbsp; End of mxc_v4l_open: v2f pix widthxheight 288 x 352&lt;/P&gt;&lt;P&gt;Because it looks like ffmpeg is using this resolution.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 15:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-custom-linux-recording-HD-video/m-p/220761#M14472</guid>
      <dc:creator>janiscoders</dc:creator>
      <dc:date>2013-01-04T15:21:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 custom linux, recording HD video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-custom-linux-recording-HD-video/m-p/220762#M14473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is better to install all the deb packages that Freescale provided.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=IMX53_11_09_LINUX_MMCODECS&amp;amp;appType=license&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;Parent_nodeId=from%20search&amp;amp;Parent_pageType=from%20search"&gt;i.MX53 Linux Multimedia Codecs Source Code&lt;/A&gt; &lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 06:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-custom-linux-recording-HD-video/m-p/220762#M14473</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-01-09T06:58:34Z</dc:date>
    </item>
  </channel>
</rss>