<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6ull qt5 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970321#M144553</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vladislav Redin,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There are some workarounds to running Qt5 on a system without GPU but it’s not supported by NXP’s BSP and you would need to make some compromises.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The thread mentioned have a comment of an user that managed to implement Qt on an embedded system without GPU, for example (hopefully they may add more information)&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/487579"&gt;https://community.nxp.com/thread/487579&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is some more information on Qt forums but using Qt5 in a system without GPU is certainly not optimal.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My apologies for the inconvenience,&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Sep 2019 20:25:21 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-09-02T20:25:21Z</dc:date>
    <item>
      <title>iMX6ull qt5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970318#M144550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How I understand the yocto project user's guide, is it totally impossible to built image with qt5 for iMX6ull evk board? I have only qt5 version of main application for my job now, how can I build linux with this application? Final two weeks i try to cross-compile it but there is no ease to understand information about how to cross-compile qt5 application for iMX6ull. Now I'm trying to build linux with qt5 for it and compile this application in the evk board, but in iMX yocto project user's guide I find this one:&lt;/P&gt;&lt;P&gt;"Builds an opensource Qt 5 image. These images are only meta-fsl-bsp-release/imx/meta-sdk&lt;BR /&gt;supported for i.MX SoC with hardware graphics. They are&lt;BR /&gt;not supported on the i.MX 6UltraLite, i.MX 6UltraLiteLite,&lt;BR /&gt;and i.MX 7Dual"&lt;/P&gt;&lt;P&gt;What should I do now? Is it really impossible to use iMX6ull with qt5 application and now I have to buy new MCU for this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 13:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970318#M144550</guid>
      <dc:creator>ATAineri</dc:creator>
      <dc:date>2019-07-25T13:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull qt5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970319#M144551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="332924" data-username="vdasvaldas09@yandex.ru" href="https://community.nxp.com/people/vdasvaldas09@yandex.ru"&gt;Vladislav Redin&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the below thread for more details on QT and imx6ULL:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/487579"&gt;i.MX 6ULL - Is Qt5 Supported?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karan Gajjar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 05:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970319#M144551</guid>
      <dc:creator>karangajjar</dc:creator>
      <dc:date>2019-07-26T05:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull qt5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970320#M144552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no fully answer in the attached link. There is only information about that is real, but no information about how to do it.&lt;/P&gt;&lt;P&gt;If I build yocto without QT and then download and install QT from dev board is this will be working even without GPU?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2019 19:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970320#M144552</guid>
      <dc:creator>ATAineri</dc:creator>
      <dc:date>2019-08-15T19:12:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull qt5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970321#M144553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vladislav Redin,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There are some workarounds to running Qt5 on a system without GPU but it’s not supported by NXP’s BSP and you would need to make some compromises.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The thread mentioned have a comment of an user that managed to implement Qt on an embedded system without GPU, for example (hopefully they may add more information)&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/487579"&gt;https://community.nxp.com/thread/487579&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is some more information on Qt forums but using Qt5 in a system without GPU is certainly not optimal.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My apologies for the inconvenience,&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 20:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/970321#M144553</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-09-02T20:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6ull qt5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/1428351#M188223</link>
      <description>&lt;DIV&gt;
&lt;P style="font-size: 12pt; font-family: 宋体; background-color: white !important; margin: 0px;" data-ogsb="white"&gt;&lt;SPAN data-ogsc="black"&gt;Actually QT5 is supported on the 6ULL. The Linux RN (seems already remove the NOTE in latest RN) and Yocto UG need to be updated.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P style="font-size: 12pt; font-family: 宋体; background-color: white !important; margin: 0px;" data-ogsb="white"&gt;&lt;SPAN data-ogsc="black"&gt;Take 5.10 Yocto release for 6ULL as example, to build QT5 into image user must bitbake the imx-image-full target. With this build, all the qt basic demo is installed and can be run. Except for the demos using OpenGLES, they're &lt;STRONG&gt;excluded&lt;/STRONG&gt; from the image.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 15 Mar 2022 09:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6ull-qt5/m-p/1428351#M188223</guid>
      <dc:creator>xinyu_chen</dc:creator>
      <dc:date>2022-03-15T09:07:09Z</dc:date>
    </item>
  </channel>
</rss>