<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Pin terminations for PCIE in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pin-terminations-for-PCIE/m-p/969500#M144395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, part of the design of a new project is using a mSATA flash drive (pSLC). The only connection to the PCIE interface is PCIE_SATA0_TX0_N/P and PCIE_SATA0RX0_N/P. Using a i.MX8QM.&lt;BR /&gt;I have worked out some of the terminations based on the reference designs provided, and the Hardware Developers Guide document, but am unsure what to do with the remaining pins. Schematic is attached. Are you able to help?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Aug 2019 04:17:13 GMT</pubDate>
    <dc:creator>pbain</dc:creator>
    <dc:date>2019-08-09T04:17:13Z</dc:date>
    <item>
      <title>Pin terminations for PCIE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-terminations-for-PCIE/m-p/969500#M144395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, part of the design of a new project is using a mSATA flash drive (pSLC). The only connection to the PCIE interface is PCIE_SATA0_TX0_N/P and PCIE_SATA0RX0_N/P. Using a i.MX8QM.&lt;BR /&gt;I have worked out some of the terminations based on the reference designs provided, and the Hardware Developers Guide document, but am unsure what to do with the remaining pins. Schematic is attached. Are you able to help?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Aug 2019 04:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-terminations-for-PCIE/m-p/969500#M144395</guid>
      <dc:creator>pbain</dc:creator>
      <dc:date>2019-08-09T04:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: Pin terminations for PCIE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-terminations-for-PCIE/m-p/969501#M144396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Note, the i.MX8 is still in preproduction stage (not fully launched yet), therefore full documentation &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;is not published.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Generally You may refer to MCIMX8QM-CPU MEK scheme and “Unused Input / Output &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Guidance” in i.MX8 QM/i.MX8 QXP Hardware Developer’s Guide regarding unused (if any)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;PCIe.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 07:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-terminations-for-PCIE/m-p/969501#M144396</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-08-12T07:24:58Z</dc:date>
    </item>
  </channel>
</rss>