<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWLAN,BT and GPS disable in Android Build</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WLAN-BT-and-GPS-disable-in-Android-Build/m-p/969092#M144325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have a custom board with IMX6 based on sabresd. for reducing memory footprint , i would like to disable wlan, bt and gps module from building. Any help is appreciated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jul 2019 11:50:37 GMT</pubDate>
    <dc:creator>anjojohn</dc:creator>
    <dc:date>2019-07-10T11:50:37Z</dc:date>
    <item>
      <title>WLAN,BT and GPS disable in Android Build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WLAN-BT-and-GPS-disable-in-Android-Build/m-p/969092#M144325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have a custom board with IMX6 based on sabresd. for reducing memory footprint , i would like to disable wlan, bt and gps module from building. Any help is appreciated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 11:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WLAN-BT-and-GPS-disable-in-Android-Build/m-p/969092#M144325</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2019-07-10T11:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: WLAN,BT and GPS disable in Android Build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WLAN-BT-and-GPS-disable-in-Android-Build/m-p/969093#M144326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi anjo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Linux Manual included in &lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga" target="_blank"&gt;Linux L4.14.98_2.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 13:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WLAN-BT-and-GPS-disable-in-Android-Build/m-p/969093#M144326</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-10T13:21:08Z</dc:date>
    </item>
  </channel>
</rss>