<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RCU Stall detected when connecting USB to server in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968339#M144198</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thank you for your prompt response. However, I just realized that I might have posted this in the wrong group. We are using Qoir T4240 Power PC based system.&lt;/P&gt;&lt;P&gt;Is it possible for you to forward this to the correct group , please?&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Pedro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jun 2019 12:21:41 GMT</pubDate>
    <dc:creator>pedro_valladare</dc:creator>
    <dc:date>2019-06-11T12:21:41Z</dc:date>
    <item>
      <title>RCU Stall detected when connecting USB to server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968337#M144196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are seeing an issue when connecting our device to a server running VMWare ESXi 6.7.0 VMKernel. If the passthrough is not enabled for the USB port, our device generates the following RCU and I cannot longer type anything at the console. If passthrough is enabled, then it works fine. If I remove the g_serial.ko module , the issue does not occur.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the output of uname -a for our system:&lt;/P&gt;&lt;P&gt;Linux (none) 4.1.8-rt8+gbd51baf #1 SMP Thu Jun 6 17:15:51 EDT 2019 ppc64 GNU/Linux&lt;/P&gt;&lt;P&gt;and the output of modinfo g_serial:&lt;/P&gt;&lt;P&gt;filename: /lib/modules/4.1.8-rt8+gbd51baf/kernel/drivers/usb/gadget/legacy/g_serial.ko&lt;BR /&gt;license: GPL&lt;BR /&gt;author: David Brownell&lt;BR /&gt;author: Al Borchers&lt;BR /&gt;description: Gadget Serial v2.4&lt;BR /&gt;depends: libcomposite&lt;BR /&gt;intree: Y&lt;BR /&gt;vermagic: 4.1.8-rt8+gbd51baf SMP mod_unload modversions&lt;BR /&gt;parm: idVendor:USB Vendor ID (ushort)&lt;BR /&gt;parm: idProduct:USB Product ID (ushort)&lt;BR /&gt;parm: bcdDevice:USB Device version (BCD) (ushort)&lt;BR /&gt;parm: iSerialNumber:SerialNumber string (charp)&lt;BR /&gt;parm: iManufacturer:USB Manufacturer string (charp)&lt;BR /&gt;parm: iProduct:USB Product string (charp)&lt;BR /&gt;parm: use_acm:Use CDC ACM, default=yes (bool)&lt;BR /&gt;parm: use_obex:Use CDC OBEX, default=no (bool)&lt;BR /&gt;parm: n_ports:number of ports to create, default=1 (uint)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;modinfo libcomposite&lt;BR /&gt;filename: /lib/modules/4.1.8-rt8+gbd51baf/kernel/drivers/usb/gadget/libcomposite.ko&lt;BR /&gt;author: David Brownell&lt;BR /&gt;license: GPL&lt;BR /&gt;depends: configfs,udc-core&lt;BR /&gt;intree: Y&lt;BR /&gt;vermagic: 4.1.8-rt8+gbd51baf SMP mod_unload modversions&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@(none):~# modinfo udc-core&lt;BR /&gt;filename: /lib/modules/4.1.8-rt8+gbd51baf/kernel/drivers/usb/gadget/udc/udc-core.ko&lt;BR /&gt;license: GPL v2&lt;BR /&gt;author: Felipe Balbi &amp;lt;balbi@ti.com&amp;gt;&lt;BR /&gt;description: UDC Framework&lt;BR /&gt;depends:&lt;BR /&gt;intree: Y&lt;BR /&gt;vermagic: 4.1.8-rt8+gbd51baf SMP mod_unload modversions&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@(none):~# modinfo configfs&lt;BR /&gt;filename: /lib/modules/4.1.8-rt8+gbd51baf/kernel/fs/configfs/configfs.ko&lt;BR /&gt;description: Simple RAM filesystem for user driven kernel subsystem configuration.&lt;BR /&gt;version: 0.0.2&lt;BR /&gt;license: GPL&lt;BR /&gt;author: Oracle&lt;BR /&gt;alias: fs-configfs&lt;BR /&gt;srcversion: BAC846119DF7A8FAD803348&lt;BR /&gt;depends:&lt;BR /&gt;intree: Y&lt;BR /&gt;vermagic: 4.1.8-rt8+gbd51baf SMP mod_unload modversions&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++&lt;/P&gt;&lt;P&gt;INFO: rcu_sched self-detected stall on CPU&lt;BR /&gt;INFO: rcu_sched self-detected stall on CPU&lt;BR /&gt; 0: (5250 ticks this GP) idle=e15/140000000000001/0 softirq=0/0 fqs=24&lt;BR /&gt; (t=5250 jiffies g=3340 c=3339 q=11378)&lt;BR /&gt;rcu_sched kthread starved for 5226 jiffies!&lt;BR /&gt;Task dump for CPU 0:&lt;BR /&gt;run R running task 0 3068 3008 0x00000004&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c0000000ca1b29d0] [c0000000000858d8] .sched_show_task+0xd8/0x164 (unreliable)&lt;BR /&gt;[c0000000ca1b2a50] [c0000000000ba970] .rcu_dump_cpu_stacks+0xd8/0x150&lt;BR /&gt;[c0000000ca1b2af0] [c0000000000c0364] .rcu_check_callbacks+0x5e0/0x8f4&lt;BR /&gt;[c0000000ca1b2c40] [c0000000000c6cec] .update_process_times+0x54/0x94&lt;BR /&gt;[c0000000ca1b2cc0] [c0000000000dc6d4] .tick_sched_handle.isra.17+0x5c/0x7c&lt;BR /&gt;[c0000000ca1b2d50] [c0000000000dc758] .tick_sched_timer+0x64/0xcc&lt;BR /&gt;[c0000000ca1b2df0] [c0000000000c7ff8] .__run_hrtimer+0xc0/0x2ec&lt;BR /&gt;[c0000000ca1b2e90] [c0000000000c85a8] .hrtimer_interrupt+0x13c/0x2f8&lt;BR /&gt;[c0000000ca1b2fa0] [c00000000001217c] .__timer_interrupt+0xa0/0x200&lt;BR /&gt;[c0000000ca1b3040] [c00000000001261c] .timer_interrupt+0x90/0xc4&lt;BR /&gt;[c0000000ca1b30c0] [c00000000001c054] exc_0x900_common+0x104/0x108&lt;BR /&gt;--- interrupt: 901 at .smp_call_function_many+0x324/0x3b8&lt;BR /&gt; LR = .smp_call_function_many+0x2e0/0x3b8&lt;BR /&gt;[c0000000ca1b33b0] [c0000000000e2f48] .smp_call_function_many+0x2c0/0x3b8 (unreliable)&lt;BR /&gt;[c0000000ca1b3470] [c00000000002ed48] .__flush_tlb_page+0x140/0x19c&lt;BR /&gt;[c0000000ca1b3530] [c00000000002c64c] .ptep_set_access_flags+0xb8/0x160&lt;BR /&gt;[c0000000ca1b35d0] [c00000000018dbb0] .do_wp_page+0x1ac/0x758&lt;BR /&gt;[c0000000ca1b36d0] [c00000000019078c] .handle_mm_fault+0xab8/0x1198&lt;BR /&gt;[c0000000ca1b37f0] [c00000000002b874] .do_page_fault+0x398/0x6cc&lt;BR /&gt;[c0000000ca1b38c0] [c00000000001d1d4] storage_fault_common+0x20/0x44&lt;BR /&gt;--- interrupt: 301 at .handle_rt_signal64+0x164/0x440&lt;BR /&gt; LR = .handle_rt_signal64+0x9c/0x440&lt;BR /&gt;[c0000000ca1b3c70] [c00000000000a974] .do_signal+0x17c/0x220&lt;BR /&gt;[c0000000ca1b3db0] [c00000000000ab98] .do_notify_resume+0x84/0x94&lt;BR /&gt;[c0000000ca1b3e30] [c000000000000c4c] .ret_from_except_lite+0x78/0x7c&lt;BR /&gt;Task dump for CPU 4:&lt;BR /&gt;run R running task 0 3111 3045 0x00000004&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c000000062f23900] [c000000001117edc] nr_cpu_ids+0x0/0x4 (unreliable)&lt;BR /&gt;Task dump for CPU 6:&lt;BR /&gt;swapper/6 R running task 0 0 1 0x00000804&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c0000000f022f9e0] [c0000000f022fa70] 0xc0000000f022fa70 (unreliable)&lt;/P&gt;&lt;P&gt;4: (1 GPs behind) idle=a65/140000000000001/0 softirq=0/0 fqs=24&lt;BR /&gt; (t=5302 jiffies g=3340 c=3339 q=11378)&lt;BR /&gt;rcu_sched kthread starved for 5279 jiffies!&lt;BR /&gt;Task dump for CPU 0:&lt;BR /&gt;run R running task 0 3068 3008 0x00000004&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c0000000ca1b3900] [c0000000ca1b39a0] 0xc0000000ca1b39a0 (unreliable)&lt;BR /&gt;Task dump for CPU 4:&lt;BR /&gt;run R running task 0 3111 3045 0x00000004&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c000000062f22f40] [c0000000000858d8] .sched_show_task+0xd8/0x164 (unreliable)&lt;BR /&gt;[c000000062f22fc0] [c0000000000ba970] .rcu_dump_cpu_stacks+0xd8/0x150&lt;BR /&gt;[c000000062f23060] [c0000000000c0364] .rcu_check_callbacks+0x5e0/0x8f4&lt;BR /&gt;[c000000062f231b0] [c0000000000c6cec] .update_process_times+0x54/0x94&lt;BR /&gt;[c000000062f23230] [c0000000000dc6d4] .tick_sched_handle.isra.17+0x5c/0x7c&lt;BR /&gt;[c000000062f232c0] [c0000000000dc758] .tick_sched_timer+0x64/0xcc&lt;BR /&gt;[c000000062f23360] [c0000000000c7ff8] .__run_hrtimer+0xc0/0x2ec&lt;BR /&gt;[c000000062f23400] [c0000000000c85a8] .hrtimer_interrupt+0x13c/0x2f8&lt;BR /&gt;[c000000062f23510] [c00000000001217c] .__timer_interrupt+0xa0/0x200&lt;BR /&gt;[c000000062f235b0] [c00000000001261c] .timer_interrupt+0x90/0xc4&lt;BR /&gt;[c000000062f23630] [c00000000001c054] exc_0x900_common+0x104/0x108&lt;BR /&gt;--- interrupt: 901 at .smp_call_function_many+0x324/0x3b8&lt;BR /&gt; LR = .smp_call_function_many+0x2e0/0x3b8&lt;BR /&gt;[c000000062f23920] [c0000000000e2f48] .smp_call_function_many+0x2c0/0x3b8 (unreliable)&lt;BR /&gt;[c000000062f239e0] [c00000000002ed48] .__flush_tlb_page+0x140/0x19c&lt;BR /&gt;[c000000062f23aa0] [c00000000002c64c] .ptep_set_access_flags+0xb8/0x160&lt;BR /&gt;[c000000062f23b40] [c00000000018dbb0] .do_wp_page+0x1ac/0x758&lt;BR /&gt;[c000000062f23c40] [c00000000019078c] .handle_mm_fault+0xab8/0x1198&lt;BR /&gt;[c000000062f23d60] [c00000000002b874] .do_page_fault+0x398/0x6cc&lt;BR /&gt;[c000000062f23e30] [c00000000001d1d4] storage_fault_common+0x20/0x44&lt;BR /&gt;Task dump for CPU 6:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 18:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968337#M144196</guid>
      <dc:creator>pedro_valladare</dc:creator>
      <dc:date>2019-06-10T18:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: RCU Stall detected when connecting USB to server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968338#M144197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hanging may be due to ddr memory errors so one can try to run ddr test and&lt;/P&gt;&lt;P&gt;rebuild image with new calibration settings found from ddr tester&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V3.00&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux&amp;nbsp; 4.1.8 version is not officially supported by nxp, one can try with nxp linux&lt;/P&gt;&lt;P&gt;from codeaurora.org/external/imx/linux-imx repository:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.98_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 23:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968338#M144197</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-10T23:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: RCU Stall detected when connecting USB to server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968339#M144198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thank you for your prompt response. However, I just realized that I might have posted this in the wrong group. We are using Qoir T4240 Power PC based system.&lt;/P&gt;&lt;P&gt;Is it possible for you to forward this to the correct group , please?&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Pedro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 12:21:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968339#M144198</guid>
      <dc:creator>pedro_valladare</dc:creator>
      <dc:date>2019-06-11T12:21:41Z</dc:date>
    </item>
    <item>
      <title>Re: RCU Stall detected when connecting USB to server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968340#M144199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I am not sure how to move this to the T4240 based processors group. Could you help to move it to the correct group please? We are still experiencing this issue.&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Pedro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 10:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968340#M144199</guid>
      <dc:creator>pedro_valladare</dc:creator>
      <dc:date>2019-06-13T10:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: RCU Stall detected when connecting USB to server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968341#M144200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems most simple is to create new thread in&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/space/2009"&gt;QorIQ Processing Platforms&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or support live chat:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/support:SUPPORTHOME" title="https://www.nxp.com/support/support:SUPPORTHOME"&gt;Support | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 22:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-Stall-detected-when-connecting-USB-to-server/m-p/968341#M144200</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-13T22:18:44Z</dc:date>
    </item>
  </channel>
</rss>