<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does Yocto Project require python, python2, or python3 ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967854#M144138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;python (short name for python2) is also required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Aug 2019 16:42:33 GMT</pubDate>
    <dc:creator>LaurentBardet</dc:creator>
    <dc:date>2019-08-27T16:42:33Z</dc:date>
    <item>
      <title>Does Yocto Project require python, python2, or python3 ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967850#M144134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From Yocto Project Quick Build, &amp;nbsp; 'Python 3.4.0 or greater'&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.yoctoproject.org/docs/2.7.1/brief-yoctoprojectqs/brief-yoctoprojectqs.html" title="https://www.yoctoproject.org/docs/2.7.1/brief-yoctoprojectqs/brief-yoctoprojectqs.html"&gt;Yocto Project Quick Build&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which Python is it referring to?&amp;nbsp; python, python2, or python3 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 19:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967850#M144134</guid>
      <dc:creator>anaseem</dc:creator>
      <dc:date>2019-08-26T19:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Does Yocto Project require python, python2, or python3 ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967851#M144135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; &lt;A _jive_internal="true" data-content-finding="Community" data-userid="326252" data-username="anaseem@trijicon.com" href="https://community.nxp.com/people/anaseem@trijicon.com"&gt;Amer Naseem&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached "&lt;STRONG&gt;Yocto project user's guide"&lt;/STRONG&gt; which can be used to setup environment for imx yocto build. You can refer the packages which are required to build yocto from &lt;STRONG&gt;section 3.1 &lt;/STRONG&gt;of&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;attached user's guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Radhika Somaiya.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 06:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967851#M144135</guid>
      <dc:creator>radhikasomaiya</dc:creator>
      <dc:date>2019-08-27T06:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: Does Yocto Project require python, python2, or python3 ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967852#M144136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"Yocto project&amp;nbsp; user's guide" directed me to "Yocto Project Quick Start" which requires to install Python 3.4.0 or greater.&amp;nbsp; Is version 3.4.0 for Phython or Python3 ?&amp;nbsp;&amp;nbsp; I think it is Phython3 because version number starts with numeral 3 ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81567iC73E70EDDE55920A/image-size/large?v=v2&amp;amp;px=999" title="package.PNG" alt="package.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81855iBD2DAF1911B4684A/image-size/large?v=v2&amp;amp;px=999" title="versions.PNG" alt="versions.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Amer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 13:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967852#M144136</guid>
      <dc:creator>anaseem</dc:creator>
      <dc:date>2019-08-27T13:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: Does Yocto Project require python, python2, or python3 ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967853#M144137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Python3, refers to python 3.4.0 or more as its update by Ubuntu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 14:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967853#M144137</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-08-27T14:25:11Z</dc:date>
    </item>
    <item>
      <title>Re: Does Yocto Project require python, python2, or python3 ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967854#M144138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;python (short name for python2) is also required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 16:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967854#M144138</guid>
      <dc:creator>LaurentBardet</dc:creator>
      <dc:date>2019-08-27T16:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: Does Yocto Project require python, python2, or python3 ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967855#M144139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;by the way, I have generated for Ubuntu Desktop 16 and currently trying 18, it seems that section 3.1 could be complemented with information;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Ubuntu 16.04 and 18.04&lt;/P&gt;&lt;P&gt;apply "Essential Yocto Project host packages",&lt;/P&gt;&lt;P&gt;then "i.MX layers host packages for a Ubuntu 14.04",&lt;/P&gt;&lt;P&gt;and finally invoke "sudo apt-get&amp;nbsp; install curl"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Ubuntu 18.04:&lt;/P&gt;&lt;P&gt;invoke also "sudo apt-get&amp;nbsp; install python"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Laurent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 16:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-Yocto-Project-require-python-python2-or-python3/m-p/967855#M144139</guid>
      <dc:creator>LaurentBardet</dc:creator>
      <dc:date>2019-08-27T16:49:33Z</dc:date>
    </item>
  </channel>
</rss>