<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: xvimagesink0: Could not initialise Xv output</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220306#M14411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is that the vpudec module, throws the data in yuv format and the Ximagesink requires the data in rgb so if I want to use them together I have to convert the image via software (ffmpegcolorspace gstreamer module) and this is very expensive for the board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently, I have gave up this approach and I am working with the frame buffer (resizing) to be able to put it within a gtk window previously designed by me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that this is not the best solution but I spent 1 week searching for information to solve my issue and nobody could help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for you answer Daiane.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jan 2013 12:00:07 GMT</pubDate>
    <dc:creator>javierrodriguez</dc:creator>
    <dc:date>2013-01-22T12:00:07Z</dc:date>
    <item>
      <title>xvimagesink0: Could not initialise Xv output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220304#M14409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a really newbie freescale user and I am getting an issue with the videosink element in gstreamer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a iMX6Q Sabrelite with a Ubuntu 12.09 within. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have modified the v4l2 kernel module in order to detect the Logitech c920 Webcam. This webcam is able to capture video with H264 hardware in HD (1080p). With a program I have captured the raw NALs into a file. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I can reproduce the video using the vpu decoder. The video plays smoothly and the system is using less than 10% of the CPU. It works fine but the gstreamer is using the v4l_sink by default. This sink puts the video directly within the framebuffer device so the system draws the image on the desktop without using a window. This is a real problem because I am working on an application that uses this and I need to display the video in a window.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to use the "xvimagesink" instead of "autovideosink" but I got this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ gst-launch-0.10 filesrc location=test.h264 ! h264parse ! vpudec ! xvimagesink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;ERROR: Pipeline doesn't want to pause.&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/GstXvImageSink:xvimagesink0: Could not initialise Xv output&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;xvimagesink.c(1428): gst_xvimagesink_get_xv_support (): /GstPipeline:pipeline0/GstXvImageSink:xvimagesink0:&lt;/P&gt;&lt;P&gt;No port available&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is very extrange. I have installed all xorg modules thate using the Xv but it does still not working. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I execute the command xvinfo, I get this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;X-Video Extension version 2.2&lt;/P&gt;&lt;P&gt;screen #0&lt;/P&gt;&lt;P&gt; no adaptors present&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;What do you think about it?.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Thank you very much.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2013 16:19:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220304#M14409</guid>
      <dc:creator>javierrodriguez</dc:creator>
      <dc:date>2013-01-03T16:19:56Z</dc:date>
    </item>
    <item>
      <title>Re: xvimagesink0: Could not initialise Xv output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220305#M14410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;have you tried using ximagesink? (and not xVimagesink)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2013 13:13:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220305#M14410</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2013-01-21T13:13:51Z</dc:date>
    </item>
    <item>
      <title>Re: xvimagesink0: Could not initialise Xv output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220306#M14411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is that the vpudec module, throws the data in yuv format and the Ximagesink requires the data in rgb so if I want to use them together I have to convert the image via software (ffmpegcolorspace gstreamer module) and this is very expensive for the board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently, I have gave up this approach and I am working with the frame buffer (resizing) to be able to put it within a gtk window previously designed by me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that this is not the best solution but I spent 1 week searching for information to solve my issue and nobody could help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for you answer Daiane.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 12:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220306#M14411</guid>
      <dc:creator>javierrodriguez</dc:creator>
      <dc:date>2013-01-22T12:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: xvimagesink0: Could not initialise Xv output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220307#M14412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for letting me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´m not used with Ubuntu rootfs, but I know totem works very well with FSL decoders, so it´s not impossible,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 17:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220307#M14412</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2013-01-22T17:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: xvimagesink0: Could not initialise Xv output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220308#M14413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was debugging totem and I discovered that totem, resize and adjust the frame buffer to the black rectangle when it playbacks a video and andjust the frame buffer to fullscreen when you configure it to view the same video in full screen. It is not a very good solution but it is a solution indeed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is very easy to adjust the output with gstreamer if you use the mfw_v4lsink video sink module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 17:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/xvimagesink0-Could-not-initialise-Xv-output/m-p/220308#M14413</guid>
      <dc:creator>javierrodriguez</dc:creator>
      <dc:date>2013-01-22T17:18:06Z</dc:date>
    </item>
  </channel>
</rss>