<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto 2.7 (Warrior) + RiotBoard ineffective reboot command in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-2-7-Warrior-RiotBoard-ineffective-reboot-command/m-p/966573#M144025</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello JY RIOT,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FSL Community BSP is supported by the Community trough the meta-freescale mailing list, you can find more details on the link below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.github.io/#contributing"&gt;https://freescale.github.io/#contributing&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perhaps it could be good that you report this, as the Warrior branch is very recent and may still have some pending bugs that are being fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also try switching to an older more mature branch to see if this problem is not present there.&lt;/P&gt;&lt;P&gt;The Riot board is manufactured and supported by Element14. So maybe they have more insights on this, I would suggest that you check their website and forums as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Sep 2019 20:28:26 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-09-09T20:28:26Z</dc:date>
    <item>
      <title>Yocto 2.7 (Warrior) + RiotBoard ineffective reboot command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-2-7-Warrior-RiotBoard-ineffective-reboot-command/m-p/966572#M144024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use the Yocto 2.7 to generate a BSP.&lt;/P&gt;&lt;P&gt;I get issue with it, this an issue with reboot, this command has almost no effect.&lt;/P&gt;&lt;P&gt;The Yocto configuration the basic configuration, here is the trace:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6dl-riotboard:~# reboot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system is going down for reboot NOW!oard (ttymxc1) (Mon Sep&amp;nbsp; 9 13:14:00 2&lt;BR /&gt;INIT: Switching to runlevel: 6&lt;BR /&gt;INIT: Sending processes the TERM signal&lt;BR /&gt;root@imx6dl-riotboard:~# Stopping OpenBSD Secure Shell server: sshdstopped /usr/sbin/sshd (pid 504)&lt;BR /&gt;.&lt;BR /&gt;Stopping system message bus: dbus.&lt;BR /&gt;Stopping syslogd/klogd: stopped syslogd (pid 513)&lt;BR /&gt;stopped klogd (pid 517)&lt;BR /&gt;done&lt;BR /&gt;Stopping random number generator daemon.&lt;BR /&gt;Deconfiguring network interfaces... ifdown: interface can0 not configured&lt;BR /&gt;ifdown: interface can1 not configured&lt;BR /&gt;done.&lt;BR /&gt;Sending all processes the TERM signal...&lt;BR /&gt;logout&lt;BR /&gt;Sending all processes the KILL signal...&lt;BR /&gt;Unmounting remote filesystems...&lt;BR /&gt;Deactivating swap...&lt;BR /&gt;Unmounting local filesystems...&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 59.402446] EXT4-fs (mmcblk0p1): re-mounted. Opts: (null)&lt;BR /&gt;Rebooting... [&amp;nbsp;&amp;nbsp; 61.560829] ci_hdrc ci_hdrc.1: remove, state 4&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.566594] usb usb1: USB disconnect, device number 1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.571862] usb 1-1: USB disconnect, device number 2&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.602306] ci_hdrc ci_hdrc.1: USB bus 1 deregistered&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.621993] reboot: Restarting system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The linux version:&lt;/P&gt;&lt;P&gt;Poky (Yocto Project Reference Distro) 2.7.1 imx6dl-riotboard ttymxc1&lt;/P&gt;&lt;P&gt;root@imx6dl-riotboard:~# uname -a&lt;BR /&gt;Linux imx6dl-riotboard 5.0.7-fslc+gc7a0e482a175 #1 SMP Mon Sep 9 09:50:35 UTC 2019 armv7l armv7l armv7l GNU/Linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the problem with the reboot command ?&lt;/P&gt;&lt;P&gt;(shutdown -r now has the same effect).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;JY RIOT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 13:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-2-7-Warrior-RiotBoard-ineffective-reboot-command/m-p/966572#M144024</guid>
      <dc:creator>jyriot</dc:creator>
      <dc:date>2019-09-09T13:42:50Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto 2.7 (Warrior) + RiotBoard ineffective reboot command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-2-7-Warrior-RiotBoard-ineffective-reboot-command/m-p/966573#M144025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello JY RIOT,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FSL Community BSP is supported by the Community trough the meta-freescale mailing list, you can find more details on the link below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.github.io/#contributing"&gt;https://freescale.github.io/#contributing&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perhaps it could be good that you report this, as the Warrior branch is very recent and may still have some pending bugs that are being fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also try switching to an older more mature branch to see if this problem is not present there.&lt;/P&gt;&lt;P&gt;The Riot board is manufactured and supported by Element14. So maybe they have more insights on this, I would suggest that you check their website and forums as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 20:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-2-7-Warrior-RiotBoard-ineffective-reboot-command/m-p/966573#M144025</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-09-09T20:28:26Z</dc:date>
    </item>
  </channel>
</rss>