<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Using touchscreen with 2 displays</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966418#M143980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I am trying to run Linux image on two displays. The displays are OK. However, only one of the displays have touchscreen. We run 2 different QT application on 2 different displays. The touchscreen interface runs, however, the touch events we make on the touchscreen display is responsive on the display that does not have touchscreen, what I mean is for example, when I touch the touchscreen coordinates 100,100 on the touchscreen display, the board thinks that I touched 100,100 coordinates on the display that does not have touchscreen.&lt;/P&gt;&lt;P&gt;I tried to change the primary display in the device tree, but no luck. I have done research on weston, again I could not find anything to redirect touch events to the touch display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is iMX8 Quad Max&lt;/P&gt;&lt;P&gt;Weston uses xwayland backend, Yocto BSP version is 4.14.98&lt;/P&gt;&lt;P&gt;What should I do to accomplish this?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Sep 2019 11:49:03 GMT</pubDate>
    <dc:creator>yavuz_mutlu</dc:creator>
    <dc:date>2019-09-24T11:49:03Z</dc:date>
    <item>
      <title>Using touchscreen with 2 displays</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966418#M143980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I am trying to run Linux image on two displays. The displays are OK. However, only one of the displays have touchscreen. We run 2 different QT application on 2 different displays. The touchscreen interface runs, however, the touch events we make on the touchscreen display is responsive on the display that does not have touchscreen, what I mean is for example, when I touch the touchscreen coordinates 100,100 on the touchscreen display, the board thinks that I touched 100,100 coordinates on the display that does not have touchscreen.&lt;/P&gt;&lt;P&gt;I tried to change the primary display in the device tree, but no luck. I have done research on weston, again I could not find anything to redirect touch events to the touch display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is iMX8 Quad Max&lt;/P&gt;&lt;P&gt;Weston uses xwayland backend, Yocto BSP version is 4.14.98&lt;/P&gt;&lt;P&gt;What should I do to accomplish this?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2019 11:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966418#M143980</guid>
      <dc:creator>yavuz_mutlu</dc:creator>
      <dc:date>2019-09-24T11:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using touchscreen with 2 displays</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966419#M143981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please also try to swap display numbers (0&amp;lt;-&amp;gt;1) in device tree and u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 09:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966419#M143981</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-09-25T09:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using touchscreen with 2 displays</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966420#M143982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I asked the same question to the wayland-devel mailing group, and they recommended that I should add WL_OUTPUT property to the udev rules for the input device. When I set the WL_OUTPUT=LVDS-2, the problem seems to be solved.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 12:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-touchscreen-with-2-displays/m-p/966420#M143982</guid>
      <dc:creator>yavuz_mutlu</dc:creator>
      <dc:date>2019-09-25T12:30:52Z</dc:date>
    </item>
  </channel>
</rss>