<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDDR RAM Configuration for the IMX6Q Custom board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966307#M143971</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;We are using IMX6 custom board with Micron &lt;STRONG&gt;MT41K256M16TW-107 AIT:P TR&lt;/STRONG&gt; DDR3L. For DDR initialization, we are trying to generate the DCD table for 2GB. Used the&amp;nbsp;MX6Q_SabreSD_DDR3_register_programming_aid_v2.3 to generate the DCD table. Generated the table but failed to boot the target device. It fails in RAM initialization. Tried several times but it didnt work. We have taken Sabresd as refernce design for our custom board. So used Sabresd configuration file and the board is booting up and working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the board went for Radiated emission test, we are observing more emissions around the DDR chip section.&lt;/P&gt;&lt;P&gt;Is it related with the operating frequency of DDR?&lt;/P&gt;&lt;P&gt;If yes, can i change the DDR operating frequency, kindly suggest or provide the procedure for modifying the operating frequency.&lt;/P&gt;&lt;P&gt;Attached is the configuration file using to boot the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be really helpful if you provide the correct DCD table for 2GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Puneeth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Sep 2019 12:58:27 GMT</pubDate>
    <dc:creator>puneethkumar_kk</dc:creator>
    <dc:date>2019-09-24T12:58:27Z</dc:date>
    <item>
      <title>DDR RAM Configuration for the IMX6Q Custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966307#M143971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;We are using IMX6 custom board with Micron &lt;STRONG&gt;MT41K256M16TW-107 AIT:P TR&lt;/STRONG&gt; DDR3L. For DDR initialization, we are trying to generate the DCD table for 2GB. Used the&amp;nbsp;MX6Q_SabreSD_DDR3_register_programming_aid_v2.3 to generate the DCD table. Generated the table but failed to boot the target device. It fails in RAM initialization. Tried several times but it didnt work. We have taken Sabresd as refernce design for our custom board. So used Sabresd configuration file and the board is booting up and working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the board went for Radiated emission test, we are observing more emissions around the DDR chip section.&lt;/P&gt;&lt;P&gt;Is it related with the operating frequency of DDR?&lt;/P&gt;&lt;P&gt;If yes, can i change the DDR operating frequency, kindly suggest or provide the procedure for modifying the operating frequency.&lt;/P&gt;&lt;P&gt;Attached is the configuration file using to boot the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be really helpful if you provide the correct DCD table for 2GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Puneeth Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2019 12:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966307#M143971</guid>
      <dc:creator>puneethkumar_kk</dc:creator>
      <dc:date>2019-09-24T12:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: DDR RAM Configuration for the IMX6Q Custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966308#M143972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Puneeth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;we are observing more emissions around the DDR chip section.&lt;/P&gt;&lt;P&gt;&amp;gt;Is it related with the operating frequency of DDR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is more related to board layout. One can look at i.MX6Q Sabre SD layout&lt;/P&gt;&lt;H3 class=""&gt;&lt;A data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emulation)" href="https://www.nxp.com/webapp/Download?colCode=iMX6Q-SABRE-SDB-DESIGNFILES&amp;amp;appType=license"&gt;Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emulation)&lt;/A&gt;&lt;/H3&gt;&lt;P&gt;also check &lt;A href="https://community.nxp.com/docs/DOC-339344"&gt;enable the spread spectrum&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For ddr tool and register programming aid usage one can look at presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331528"&gt;DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 00:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966308#M143972</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-25T00:58:06Z</dc:date>
    </item>
    <item>
      <title>Re: DDR RAM Configuration for the IMX6Q Custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966309#M143973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;DIV class=""&gt;Thank you for your quick response.&lt;/DIV&gt;&lt;P&gt;i am checking on this and I'll get back to you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Puneeth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 13:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-RAM-Configuration-for-the-IMX6Q-Custom-board/m-p/966309#M143973</guid>
      <dc:creator>puneethkumar_kk</dc:creator>
      <dc:date>2019-09-25T13:13:32Z</dc:date>
    </item>
  </channel>
</rss>