<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: SPI Slave Example</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965333#M143838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply Igor, but, this is all?&lt;/P&gt;&lt;P&gt;If you use the spidev, I believe that I will need a application to supply the data to export in SPI bus to Master. It is not like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jun 2019 06:15:04 GMT</pubDate>
    <dc:creator>jzabalza</dc:creator>
    <dc:date>2019-06-11T06:15:04Z</dc:date>
    <item>
      <title>SPI Slave Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965331#M143836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Document IMXLXRN Release Notes Rev. L4.14.98-2.0.0_ga, 05/2019 I can read that NXP BSP has SPI slave support (Table 8. Supported features)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there some example code application or driver using this feature?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 15:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965331#M143836</guid>
      <dc:creator>jzabalza</dc:creator>
      <dc:date>2019-06-10T15:05:04Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Slave Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965332#M143837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at linux/arch/arm/boot/dts/imx6ul-14x14-evk-ecspi-slave.dts example:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk-ecspi-slave.dts?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk-ecspi-slave.dts?h=imx_4.14.98_2.0.0_ga"&gt;imx6ul-14x14-evk-ecspi-slave.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 00:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965332#M143837</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-11T00:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Slave Example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965333#M143838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply Igor, but, this is all?&lt;/P&gt;&lt;P&gt;If you use the spidev, I believe that I will need a application to supply the data to export in SPI bus to Master. It is not like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 06:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Example/m-p/965333#M143838</guid>
      <dc:creator>jzabalza</dc:creator>
      <dc:date>2019-06-11T06:15:04Z</dc:date>
    </item>
  </channel>
</rss>