<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAbout i.MX7D DDR Controller Configuration Spreadsheet</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-i-MX7D-DDR-Controller-Configuration-Spreadsheet/m-p/964248#M143687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Community&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In order to perform LPDDR3 calibration from i.MX7d, I am editing the attached spreadsheet.&lt;BR /&gt;I have two questions.&lt;BR /&gt;(1) The max frequency is 533MHz.&lt;BR /&gt;In that case, the READ Latency is 8, the Write Latency is 4, and it is listed in the DDR data sheet.&lt;BR /&gt;I have to change line numbers 114 and 115 in the attachment sheet “Register Configuration”.&lt;BR /&gt;There is a statement that the value will be maintained and not changed as shown below.&lt;BR /&gt;Can I change this?&lt;BR /&gt;"On Register Configuration Tab, an unshaded cell means that the value should remain as is and should not be modified.In these cases, the settings are provided for completeness."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) RD2PRE on line 109 of attached sheet "Register Configuration"&lt;BR /&gt;The formula “LPDDR3: BL / 2 + max (tRTP, 4)-4” is listed in the Notes column.&lt;BR /&gt;However, the cell D109 does not have such a formula.&lt;BR /&gt;Can I keep this as it is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Reguads,&lt;/P&gt;&lt;P&gt;Goto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Aug 2019 08:16:35 GMT</pubDate>
    <dc:creator>goto11</dc:creator>
    <dc:date>2019-08-23T08:16:35Z</dc:date>
    <item>
      <title>About i.MX7D DDR Controller Configuration Spreadsheet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-i-MX7D-DDR-Controller-Configuration-Spreadsheet/m-p/964248#M143687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Community&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In order to perform LPDDR3 calibration from i.MX7d, I am editing the attached spreadsheet.&lt;BR /&gt;I have two questions.&lt;BR /&gt;(1) The max frequency is 533MHz.&lt;BR /&gt;In that case, the READ Latency is 8, the Write Latency is 4, and it is listed in the DDR data sheet.&lt;BR /&gt;I have to change line numbers 114 and 115 in the attachment sheet “Register Configuration”.&lt;BR /&gt;There is a statement that the value will be maintained and not changed as shown below.&lt;BR /&gt;Can I change this?&lt;BR /&gt;"On Register Configuration Tab, an unshaded cell means that the value should remain as is and should not be modified.In these cases, the settings are provided for completeness."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) RD2PRE on line 109 of attached sheet "Register Configuration"&lt;BR /&gt;The formula “LPDDR3: BL / 2 + max (tRTP, 4)-4” is listed in the Notes column.&lt;BR /&gt;However, the cell D109 does not have such a formula.&lt;BR /&gt;Can I keep this as it is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Reguads,&lt;/P&gt;&lt;P&gt;Goto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2019 08:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-i-MX7D-DDR-Controller-Configuration-Spreadsheet/m-p/964248#M143687</guid>
      <dc:creator>goto11</dc:creator>
      <dc:date>2019-08-23T08:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: About i.MX7D DDR Controller Configuration Spreadsheet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-i-MX7D-DDR-Controller-Configuration-Spreadsheet/m-p/964249#M143688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; It is possible to modify values in lines 114, 115, using column "Number of DDR Clock Cycles or time (ns)".&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;2.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp; The Excel formula of cell D109 is just recommendation (typical). Customers can use exact calculations,&lt;/P&gt;&lt;P class=""&gt;if needed in their design.&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 05:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-i-MX7D-DDR-Controller-Configuration-Spreadsheet/m-p/964249#M143688</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-08-26T05:49:22Z</dc:date>
    </item>
  </channel>
</rss>