<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220004#M14345</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Max &amp;amp; &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Gerard,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please follow below link to updae GPU lib and driver, and then retry. if problem is still there, please feedback here.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-94481"&gt;https://community.freescale.com/docs/DOC-94481&lt;/A&gt;&lt;/P&gt;&lt;H1 style="margin: 0 100px 0 0; padding-left: 32px; font-size: 26px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;/H1&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fuzhen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2013 07:16:00 GMT</pubDate>
    <dc:creator>fuzhenlin</dc:creator>
    <dc:date>2013-04-24T07:16:00Z</dc:date>
    <item>
      <title>Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/219997#M14338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a design based on the FS sabresd board but instead of 1GB it has 2GB DDR3 memory (also using 64-bit wide bus and a single chip select using 4 x 256Mbx16 DDR3 SDRAM parts - instead of the 4 x 128Mbx16 DDR3 parts used on the FS sabresd SDP).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tried many different settings for CS0_END (correct one should be 47h = 3F+8 according to FS FAE IN USA). We also set the correct max memory size in the sabresd kernel file (changed from 1u * 1024 * 1024 * 1024 to 2u * 1024 *1024 * 1024).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also set register 0x021b0000 to 0x841a0000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These settings pass the FS DDR_STRESS_TESTER 2GB memory tests with flying colors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BUT when we boot into Android V13.4 BSP, Android boots up OK and correctly "sees" the 2GB of DDR3 memory BUT when one moves out of the Android lock screen into any other screen (eg: any settings screen) the ouse pointer leaves trailing pounters all over the show which never get erased. When we set memory size back to 1GB settings everythig works great. I have seem 1 other report from someone in China with the same problem and same configuratuon, so we are not alone. Have a look at: &lt;A href="https://community.nxp.com/message/308827"&gt;any one use 2GB ddr3 with imx6q android bsp?&lt;/A&gt; (he also attaches a great screenshot of this "trailing mouse pointer" problem - which is 100% the same as as we are seeing). Same problem occurs on both dual and quad i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only reason I started a new thread here is in the hope that this title will attract a few more hits than the already good question from the gentleman in China.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone successfully booted Android BSP V13.4 on an iMX6 using 2GB DDR3 memory with a 64-bot wide bus and single chip select, etc.&lt;/P&gt;&lt;P&gt;URGENTLY NEED SOME HELP!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gerard Bucas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2013 02:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/219997#M14338</guid>
      <dc:creator>gerardbucas</dc:creator>
      <dc:date>2013-01-03T02:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/219998#M14339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just looked at the mx6qsabreauto schematics and it seems to have exactly the same DDR3 configuration that you need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Jan 2013 12:58:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/219998#M14339</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-01-05T12:58:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/219999#M14340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And here is the DDR3 setup for this board that you can reference:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6q_sabreauto/flash_header.S?h=imx_v2009.08_12.10.02" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6q_sabreauto/flash_header.S?h=imx_v2009.08_12.10.02"&gt;http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6q_sabreauto/flash_header.S?h=imx_v2009.08_12.10.02&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Jan 2013 13:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/219999#M14340</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-01-05T13:06:31Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220000#M14341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, we followed your suggestion to use mx6qSABREAUTO flash_header.S, and now it is 2GB DDR#, but still has "&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;trailing mouse pointer&lt;/SPAN&gt;" problem. Have you any idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chi-Chung Chen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2013 05:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220000#M14341</guid>
      <dc:creator>omar_ccc</dc:creator>
      <dc:date>2013-02-20T05:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220001#M14342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;screenshot from ddms, there is no "&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;trailing mouse pointer&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119031iD01002D6A12DC803/image-size/large?v=v2&amp;amp;px=999" title="device-2013-02-21-103517.png" alt="device-2013-02-21-103517.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;photo from my phone,you could see the&amp;nbsp; "&lt;SPAN style="background-color: #ffffff; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;trailing mouse pointer&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119032iE6A76955971E5974/image-size/large?v=v2&amp;amp;px=999" title="IMG_20130221_103458.jpg" alt="IMG_20130221_103458.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does any one could give me some idea about this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 06:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220001#M14342</guid>
      <dc:creator>MaxChou</dc:creator>
      <dc:date>2013-02-21T06:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220002#M14343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MX6 SabreAI&amp;nbsp; supports 2G memory. 2G memory configuration was tested with Android JellyBean on MX6 SabreAI board.&amp;nbsp; The issue was not observed. &lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Can you please check whether&amp;nbsp; framebuffer region is overlapped with other reserved memory? Such as GPU memory etc.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2013 03:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220002#M14343</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-03-19T03:14:01Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220003#M14344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;Dear Gerard Bucas:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I also encountered &lt;SPAN class="hps"&gt;the same problem.&lt;SPAN class="long_text short_text" lang="en"&gt;&lt;SPAN&gt;Do&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;not&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;know if you&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;solved the problem?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2013 06:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220003#M14344</guid>
      <dc:creator>bingking88</dc:creator>
      <dc:date>2013-04-18T06:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220004#M14345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Max &amp;amp; &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Gerard,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please follow below link to updae GPU lib and driver, and then retry. if problem is still there, please feedback here.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-94481"&gt;https://community.freescale.com/docs/DOC-94481&lt;/A&gt;&lt;/P&gt;&lt;H1 style="margin: 0 100px 0 0; padding-left: 32px; font-size: 26px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;/H1&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fuzhen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2013 07:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220004#M14345</guid>
      <dc:creator>fuzhenlin</dc:creator>
      <dc:date>2013-04-24T07:16:00Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220005#M14346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Binking and Max,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Fuzhen and I can't reproduce the issue on our sabreAI board, could you do more try to help us analysis the issue.&lt;/P&gt;&lt;P&gt;First I want to disable 2D hwcomposer to have a try, please follow below steps in console:&lt;/P&gt;&lt;P&gt;1. root@android:/ # cd system/lib/hw/&lt;/P&gt;&lt;P&gt;2. root@android:/system/lib/hw # mount -o remount rw /system&lt;/P&gt;&lt;P&gt;3. root@android:/system/lib/hw # mv hwcomposer_viv.imx6.so hwcomposer_viv.imx6.so.bak&lt;/P&gt;&lt;P&gt;4. &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;root@android:/system/lib/hw # sync&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;5. root@android:/system/lib/hw # reboot&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2013 05:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220005#M14346</guid>
      <dc:creator>LiuXuegang</dc:creator>
      <dc:date>2013-04-26T05:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problem configuring 2GB DDR3 on i.MX6 Android BSP?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220006#M14347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;Summary the conclusion:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;1. &lt;/SPAN&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;Confirmed the trailing mouse issue not exist if disable android swap rectangle feature. &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;2. &lt;/SPAN&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;GPU reserved memory address region should be limited within 2G as GPU command buffer use reserved memory and it can’t accept virtual memory. &lt;/SPAN&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;Our kernel code has this limit memblock_alloc_base(imx6q_gpu_pdata.reserved_mem_size,SZ_4K,&lt;STRONG style="font-style: inherit; font-family: inherit;"&gt;SZ_2G) &lt;/STRONG&gt;for 2G DDR device for example FSL SabreAI reference board.&lt;/SPAN&gt;&lt;SPAN style="font-style: inherit; font-size: 10pt; font-family: inherit;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;SPAN style="font-style: inherit; font-size: 10pt; font-family: inherit;"&gt;3. &lt;/SPAN&gt;&lt;SPAN style="font-style: inherit; font-size: 12pt; font-family: inherit;"&gt;fb0base address can be set to &amp;gt; 2G, but there will be some performance drop, so suggest customer not set fb0base &amp;gt; 2G.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2013 06:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-configuring-2GB-DDR3-on-i-MX6-Android-BSP/m-p/220006#M14347</guid>
      <dc:creator>LiuXuegang</dc:creator>
      <dc:date>2013-05-09T06:33:20Z</dc:date>
    </item>
  </channel>
</rss>