<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 initialization and start-up scripts</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-initialization-and-start-up-scripts/m-p/219753#M14324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;Trace 32 init script for i.MX6x are attached :&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; attach_core1.cmm ---- Attach only one core, core0 &lt;BR /&gt; &lt;BR /&gt; attach_4core.cmm ---- Attach all 4 core4 &lt;BR /&gt; &lt;BR /&gt; DDR initialization scripts:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; MX61_init_LPDDR2_528MHz_Micron_1_00.cmm ---- initialize LPDDR2 2-ch &lt;BR /&gt; running at 528MHz &lt;BR /&gt; &lt;BR /&gt; MX61_init_CPUDDR3_528MHz_64bit_1_04.cmm --- initialize DDR3&amp;nbsp; 64bits at &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;528MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;Please notice that the DDR initialization scripts are for Freescale reference &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;board, as for customers board, some parameter maybe needed to be tuned.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2013 07:32:42 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-01-09T07:32:42Z</dc:date>
    <item>
      <title>i.MX6 initialization and start-up scripts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-initialization-and-start-up-scripts/m-p/219752#M14323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working on Custom i.MX6S hardware for bring-up. For flashing purpose it is important that USB devices should be enumerated and board should be identified as a USB device when connected to host. Is that correct? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use MFG utility from Freescale to flash the images. Switch has been set to USB OTG boot.When hardware is connected to host via USB OTG cable, hardware enumeration for USB doesn't show up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone used the Lauterbach debugger for i.MX6 boards (may be SabreLite board). Are the init scripts for i.MX6S available for Lauterbach debugger to debug the i.mx6 start-up sequence?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;kk&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2013 09:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-initialization-and-start-up-scripts/m-p/219752#M14323</guid>
      <dc:creator>KaushikRKarandi</dc:creator>
      <dc:date>2013-01-02T09:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 initialization and start-up scripts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-initialization-and-start-up-scripts/m-p/219753#M14324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;Trace 32 init script for i.MX6x are attached :&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; attach_core1.cmm ---- Attach only one core, core0 &lt;BR /&gt; &lt;BR /&gt; attach_4core.cmm ---- Attach all 4 core4 &lt;BR /&gt; &lt;BR /&gt; DDR initialization scripts:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; MX61_init_LPDDR2_528MHz_Micron_1_00.cmm ---- initialize LPDDR2 2-ch &lt;BR /&gt; running at 528MHz &lt;BR /&gt; &lt;BR /&gt; MX61_init_CPUDDR3_528MHz_64bit_1_04.cmm --- initialize DDR3&amp;nbsp; 64bits at &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;528MHz&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;Please notice that the DDR initialization scripts are for Freescale reference &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;board, as for customers board, some parameter maybe needed to be tuned.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2013 07:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-initialization-and-start-up-scripts/m-p/219753#M14324</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-01-09T07:32:42Z</dc:date>
    </item>
  </channel>
</rss>