<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX28 Has anyone made a package of the bootstream? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-Has-anyone-made-a-package-of-the-bootstream/m-p/959187#M143198</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since the bootstream is the binary monolitic file that contains the initial hardware configuration section, the bootloader and the kernel code, there is no way to make a rpm package of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jun 2019 07:03:02 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2019-06-28T07:03:02Z</dc:date>
    <item>
      <title>iMX28 Has anyone made a package of the bootstream?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-Has-anyone-made-a-package-of-the-bootstream/m-p/959186#M143197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are working with the iMX28 with Yocto (morty) building the 4.1 kernel and using the linux.sb &amp;amp; linux.sdcard output to burn a µSD image.&amp;nbsp; We use rpm packages to do over-the-air updates to are target device but the bootstream is not packaged by morty.&amp;nbsp; I can arrange for the bootstream to be left in "tmp/deploy/images/&amp;lt;machine&amp;gt;" but I don't know how to get the packaging system to make a package of it, preferably named with the same version number as the kernel and it's modules.&lt;/P&gt;&lt;P&gt;Has anyone done this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 03:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-Has-anyone-made-a-package-of-the-bootstream/m-p/959186#M143197</guid>
      <dc:creator>colinmoloney</dc:creator>
      <dc:date>2019-06-24T03:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 Has anyone made a package of the bootstream?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-Has-anyone-made-a-package-of-the-bootstream/m-p/959187#M143198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since the bootstream is the binary monolitic file that contains the initial hardware configuration section, the bootloader and the kernel code, there is no way to make a rpm package of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 07:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-Has-anyone-made-a-package-of-the-bootstream/m-p/959187#M143198</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-06-28T07:03:02Z</dc:date>
    </item>
  </channel>
</rss>