<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: BT656 Debugging on IMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BT656-Debugging-on-IMX6/m-p/957445#M143046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Úmit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid there is no status register indicating detection the SAV/EVA code.&amp;nbsp; Since IPU data is handled by IDMAC, one can try to check RM sect.37.4.2.14 IDMAC's internal events, check IPUx_INT_CTRL indicating End Of Frame of Channel #n.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Oct 2019 16:26:25 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-10-29T16:26:25Z</dc:date>
    <item>
      <title>BT656 Debugging on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BT656-Debugging-on-IMX6/m-p/957444#M143045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to see the EAV and SAV bytes on sw for IMX6, in which file on kernel or userspace i need to focus?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually i wrote down a driver on platform mxc folder and it is not working. Now i want to debug the pixel clock(i want to read it on sw driver) and EAC-SAV to make sure driver is working properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Umit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 13:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BT656-Debugging-on-IMX6/m-p/957444#M143045</guid>
      <dc:creator>umit_kayacik</dc:creator>
      <dc:date>2019-10-23T13:21:45Z</dc:date>
    </item>
    <item>
      <title>Re: BT656 Debugging on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BT656-Debugging-on-IMX6/m-p/957445#M143046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Úmit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid there is no status register indicating detection the SAV/EVA code.&amp;nbsp; Since IPU data is handled by IDMAC, one can try to check RM sect.37.4.2.14 IDMAC's internal events, check IPUx_INT_CTRL indicating End Of Frame of Channel #n.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 16:26:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BT656-Debugging-on-IMX6/m-p/957445#M143046</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-10-29T16:26:25Z</dc:date>
    </item>
  </channel>
</rss>