<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: configure static ip on imx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219530#M14304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jan 2013 14:53:05 GMT</pubDate>
    <dc:creator>davidshoham</dc:creator>
    <dc:date>2013-01-02T14:53:05Z</dc:date>
    <item>
      <title>configure static ip on imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219528#M14302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I installed the basic rootfs from the"L3.0.35_12.09.01_GA_images_MX6Q" packages. I am trying to configure a static ip permanently and have n idea how to do this. In the meantime I am configuring the ip with 'ifconfig' every time I switch on the card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;David.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jan 2013 13:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219528#M14302</guid>
      <dc:creator>davidshoham</dc:creator>
      <dc:date>2013-01-01T13:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: configure static ip on imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219529#M14303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can pass the IP you want in the kernel command line (from the bootloader) like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ip=192.168.1.102:192.168.1.101&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;,where&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;192.168.1.101: is the serverip IP address&lt;/P&gt;&lt;P&gt;192.168.1.102: is the target (mx6 board) IP address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2013 01:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219529#M14303</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-01-02T01:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: configure static ip on imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219530#M14304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2013 14:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/configure-static-ip-on-imx6/m-p/219530#M14304</guid>
      <dc:creator>davidshoham</dc:creator>
      <dc:date>2013-01-02T14:53:05Z</dc:date>
    </item>
  </channel>
</rss>