<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCIE on iMX6Q problems in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957215#M143015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Minh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check with other cards if they will be detected, also look at below suggestions&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/383799"&gt;i.MX6 “PHY link never came up”&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://forum.variscite.com/viewtopic.php?t=109" title="http://forum.variscite.com/viewtopic.php?t=109"&gt;VAR-MX6Custom board PCIe phy does not come up - Variscite Forums&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://gitlab.denx.de/u-boot/u-boot/commit/5a82e1a21d1229e7e3d1c64187735794019e9a1b" title="https://gitlab.denx.de/u-boot/u-boot/commit/5a82e1a21d1229e7e3d1c64187735794019e9a1b"&gt;pci: mx6: fix occasional link failures (5a82e1a2) · Commits · U-Boot / U-Boot · GitLab&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also phytec uses own bsps so may be relevant to post issue on its forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2019 23:42:49 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-07-23T23:42:49Z</dc:date>
    <item>
      <title>PCIE on iMX6Q problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957214#M143014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to implement a Wlan card from LAIRD to a custom iMX6Q from Phytec based on distro fsl-imx-xwayland. The meta-laird-cp wifi driver and backport is already included in bb layer and conf file. On the booting, I think PCIe has some problems:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.550313] imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.550727] imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.550760] pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0xffff]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.550786] pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.550814] pci_bus 0000:00: root bus resource [bus 00-ff]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.551636] PCI: bus0: Fast back to back transfers disabled&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.551912] PCI: bus1: Fast back to back transfers enabled&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.552110] pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.552151] pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.552179] pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.552595] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PCI host seem to be can not detected because there is no mapping for PCI IO and PCI MEM. The signal PME is also interrupt.&lt;/P&gt;&lt;P&gt;When I test with command lspci -v, system can not detect the wlan card, just only the PCI bridge:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;00:00.0 PCI bridge: Synopsys, Inc. Device abcd (rev 01) (prog-if 00 [Normal decode])&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Flags: bus master, fast devsel, latency 0, IRQ 298&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Memory at 01000000 (32-bit, non-prefetchable) [size=1M]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bus: primary=00, secondary=01, subordinate=ff, sec-latency=0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I/O behind bridge: None&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Memory behind bridge: None&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Prefetchable memory behind bridge: None&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [virtual] Expansion ROM at 01100000 [disabled] [size=64K]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capabilities: [40] Power Management version 3&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capabilities: [50] MSI: Enable+ Count=1/1 Maskable+ 64bit+&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capabilities: [70] Express Root Port (Slot-), MSI 00&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capabilities: [100] Advanced Error Reporting&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capabilities: [140] Virtual Channel&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kernel driver in use: pcieport&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I configure the PCI driver correct? Anyone have idea about this. Hope that you can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Best Regards,&lt;/P&gt;&lt;P&gt;Minh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 12:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957214#M143014</guid>
      <dc:creator>minhnguyen</dc:creator>
      <dc:date>2019-07-23T12:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE on iMX6Q problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957215#M143015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Minh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check with other cards if they will be detected, also look at below suggestions&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/383799"&gt;i.MX6 “PHY link never came up”&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://forum.variscite.com/viewtopic.php?t=109" title="http://forum.variscite.com/viewtopic.php?t=109"&gt;VAR-MX6Custom board PCIe phy does not come up - Variscite Forums&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://gitlab.denx.de/u-boot/u-boot/commit/5a82e1a21d1229e7e3d1c64187735794019e9a1b" title="https://gitlab.denx.de/u-boot/u-boot/commit/5a82e1a21d1229e7e3d1c64187735794019e9a1b"&gt;pci: mx6: fix occasional link failures (5a82e1a2) · Commits · U-Boot / U-Boot · GitLab&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also phytec uses own bsps so may be relevant to post issue on its forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 23:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957215#M143015</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-23T23:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE on iMX6Q problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957216#M143016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help, now I can integrate the driver of wlan card and the wlan card also regconize on the PCI lists device through command&lt;STRONG&gt; lspci -v.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In the boot logs file have these issues:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ OK ] Started Rebuil[ 5.736692] Loading modules backported from Linux version LRD-REL-7.0.0.52-0-ga7b66f2&lt;BR /&gt;d Journal Catalog.&lt;BR /&gt;[ 5.746004] Backport generated by backports.git LRD-REL-7.0.0.52-0-g6748ad4&lt;BR /&gt;[ 5.784275] lrdmwl: disagrees about version of symbol ieee80211_queue_stopped&lt;BR /&gt;[ 5.791448] lrdmwl: Unknown symbol ieee80211_queue_stopped (err -22)&lt;BR /&gt;[ 5.802784] coda 2040000.vpu: Direct firmware load for v4l-coda960-imx6q.bin failed with error -2&lt;BR /&gt;[ 5.810906] lrdmwl: disagrees about version of symbol ieee80211_stop_tx_ba_session&lt;BR /&gt;[ 5.810912] lrdmwl: Unknown symbol ieee80211_stop_tx_ba_session (err -22)&lt;BR /&gt;[ 5.810924] lrdmwl: disagrees about version of symbol ieee80211_start_tx_ba_cb_irqsafe&lt;BR /&gt;[ 5.810928] lrdmwl: Unknown symbol ieee80211_start_tx_ba_cb_irqsafe (err -22)&lt;BR /&gt;[ 5.810943] lrdmwl: disagrees about version of symbol ieee80211_connection_loss&lt;BR /&gt;[ 5.810946] lrdmwl: Unknown symbol ieee80211_connection_loss (err -22)&lt;BR /&gt;[ 5.810958] lrdmwl: disagrees about version of symbol ieee80211_report_wowlan_wakeup&lt;BR /&gt;[ 5.810970] lrdmwl: Unknown symbol ieee80211_report_wowlan_wakeup (err -22)&lt;BR /&gt;[ 5.821480] lrdmwl: disagrees about version of symbol ieee80211_free_hw&lt;BR /&gt;[ 5.821486] lrdmwl: Unknown symbol ieee80211_free_hw (err -22)&lt;BR /&gt;[ 5.821517] lrdmwl: disagrees about version of symbol ieee80211_start_tx_ba_session&lt;BR /&gt;[ 5.821522] lrdmwl: Unknown symbol ieee80211_start_tx_ba_session (err -22)&lt;BR /&gt;[ 5.821536] lrdmwl: disagrees about version of symbol regulatory_hint&lt;BR /&gt;[ 5.821540] lrdmwl: Unknown symbol regulatory_hint (err -22)&lt;BR /&gt;[ 5.821576] lrdmwl: disagrees about version of symbol ieee80211_register_hw&lt;BR /&gt;[ 5.821579] lrdmwl: Unknown symbol ieee80211_register_hw (err -22)&lt;BR /&gt;[ 5.821588] lrdmwl: disagrees about version of symbol ieee80211_restart_hw&lt;BR /&gt;[ 5.821591] lrdmwl: Unknown symbol ieee80211_restart_hw (err -22)&lt;BR /&gt;[ 5.821613] lrdmwl: Unknown symbol cfg80211_find_ie_match (err 0)&lt;BR /&gt;[ 5.821628] lrdmwl: disagrees about version of symbol ieee80211_wake_queue&lt;BR /&gt;[ 5.821631] lrdmwl: Unknown symbol ieee80211_wake_queue (err -22)&lt;BR /&gt;[ 5.821697] lrdmwl: disagrees about version of symbol __cfg80211_alloc_reply_skb&lt;BR /&gt;[ 5.821701] lrdmwl: Unknown symbol __cfg80211_alloc_reply_skb (err -22)&lt;BR /&gt;[ 5.821736] lrdmwl: disagrees about version of symbol ieee80211_stop_tx_ba_cb_irqsafe&lt;BR /&gt;[ 5.821739] lrdmwl: Unknown symbol ieee80211_stop_tx_ba_cb_irqsafe (err -22)&lt;BR /&gt;[ 5.821756] lrdmwl: disagrees about version of symbol wiphy_to_ieee80211_hw&lt;BR /&gt;[ 5.821759] lrdmwl: Unknown symbol wiphy_to_ieee80211_hw (err -22)&lt;BR /&gt;[ 5.821821] lrdmwl: disagrees about version of symbol ieee80211_remain_on_channel_expired&lt;BR /&gt;[ 5.821824] lrdmwl: Unknown symbol ieee80211_remain_on_channel_expired (err -22)&lt;BR /&gt;[ 5.821867] lrdmwl: disagrees about version of symbol ieee80211_wake_queues&lt;BR /&gt;[ 5.821870] lrdmwl: Unknown symbol ieee80211_wake_queues (err -22)&lt;BR /&gt;[ 5.821900] lrdmwl: disagrees about version of symbol ieee80211_alloc_hw_nm&lt;BR /&gt;[ 5.821903] lrdmwl: Unknown symbol ieee80211_alloc_hw_nm (err -22)&lt;BR /&gt;[ 5.821933] lrdmwl: disagrees about version of symbol cfg80211_vendor_cmd_reply&lt;BR /&gt;[ 5.821936] lrdmwl: Unknown symbol cfg80211_vendor_cmd_reply (err -22)&lt;BR /&gt;[ 5.821960] lrdmwl: disagrees about version of symbol ieee80211_tx_status&lt;BR /&gt;[ 5.821963] lrdmwl: Unknown symbol ieee80211_tx_status (err -22)&lt;BR /&gt;[ 5.821969] lrdmwl: disagrees about version of symbol ieee80211_stop_queue&lt;BR /&gt;[ 5.821971] lrdmwl: Unknown symbol ieee80211_stop_queue (err -22)&lt;BR /&gt;[ 5.821987] lrdmwl: disagrees about version of symbol ieee80211_ready_on_channel&lt;BR /&gt;[ 5.821990] lrdmwl: Unknown symbol ieee80211_ready_on_channel (err -22)&lt;BR /&gt;[ 5.821995] lrdmwl: disagrees about version of symbol ieee80211_stop_queues&lt;BR /&gt;[ 5.821998] lrdmwl: Unknown symbol ieee80211_stop_queues (err -22)&lt;BR /&gt;[ 5.822034] lrdmwl: disagrees about version of symbol ieee80211_channel_to_frequency&lt;BR /&gt;[ 5.822037] lrdmwl: Unknown symbol ieee80211_channel_to_frequency (err -22)&lt;BR /&gt;[ 5.822043] lrdmwl: disagrees about version of symbol ieee80211_unregister_hw&lt;BR /&gt;[ 5.822046] lrdmwl: Unknown symbol ieee80211_unregister_hw (err -22)&lt;BR /&gt;[ 5.822058] lrdmwl: disagrees about version of symbol ieee80211_beacon_get_tim&lt;BR /&gt;[ 5.822061] lrdmwl: Unknown symbol ieee80211_beacon_get_tim (err -22)&lt;BR /&gt;[ 5.822081] lrdmwl: disagrees about version of symbol ieee80211_radar_detected&lt;BR /&gt;[ 5.822084] lrdmwl: Unknown symbol ieee80211_radar_detected (err -22)&lt;BR /&gt;[ 5.822134] lrdmwl: disagrees about version of symbol ieee80211_csa_finish&lt;BR /&gt;[ 5.822137] lrdmwl: Unknown symbol ieee80211_csa_finish (err -22)&lt;BR /&gt;[ 5.822153] lrdmwl: Unknown symbol ieee80211_rx_napi (err 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea about these Errors. Phytec BSP do not implement the fsl_imx_gpu direct Frame Buffer that I need to develop the software based on OpenGL ES. So that's why I make a BSP based on the fsl-imx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Minh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 08:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/957216#M143016</guid>
      <dc:creator>minhnguyen</dc:creator>
      <dc:date>2019-08-01T08:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE on iMX6Q problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/1208478#M167437</link>
      <description>&lt;P&gt;John from Laird Connectivity here.&lt;/P&gt;&lt;P&gt;Just for future reference, these errors are caused either by the backported driver being used with in-tree mac80211 and cfg80211 or backports was built against a different kernel than the one running on the host here.&lt;/P&gt;&lt;P&gt;If you are experiencing errors similar to these, the kernel will have to be reconfigured/recompiled with the wireless subsystem removed and backports built against that kernel and deployed on the host with the new kernel. Laird Connectivity provides an external layer&amp;nbsp;for building the driver and firmware with custom Yocto images. Please see our layer here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/LairdCP/meta-laird-cp" target="_blank" rel="noopener"&gt;https://github.com/LairdCP/meta-laird-cp&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And if support is needed, please click on the button "Open a Support Ticket" found in the link below.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lairdconnect.com/resources/support" target="_blank" rel="noopener"&gt;https://www.lairdconnect.com/resources/support&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 19:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-on-iMX6Q-problems/m-p/1208478#M167437</guid>
      <dc:creator>johnnosky</dc:creator>
      <dc:date>2021-01-07T19:15:00Z</dc:date>
    </item>
  </channel>
</rss>