<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ATK - BI Swap / BBT set incorrectly in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957123#M142989</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a working iMX27 design using Micron NAND with Windows CE.&amp;nbsp; Using advanced toolkit 1.71 to load code the procedure is to set the "Program" and "BI Swap" operation flags to program XLDR and EBOOT and all works well.&amp;nbsp; Unfortunately, for a couple boards the "BBT" flag was set instead of&amp;nbsp;&lt;SPAN&gt;"BI Swap" (something the manual warns against doing).&amp;nbsp; We tried reprogramming them with the correct settings and while they program OK they do not boot.&amp;nbsp;&amp;nbsp;Tried a full erase, etc., no luck.&amp;nbsp; Any way to recover these boards using&amp;nbsp;ATK or do I need to replace the FLASH part?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Aug 2019 14:24:17 GMT</pubDate>
    <dc:creator>ambw</dc:creator>
    <dc:date>2019-08-06T14:24:17Z</dc:date>
    <item>
      <title>ATK - BI Swap / BBT set incorrectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957123#M142989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a working iMX27 design using Micron NAND with Windows CE.&amp;nbsp; Using advanced toolkit 1.71 to load code the procedure is to set the "Program" and "BI Swap" operation flags to program XLDR and EBOOT and all works well.&amp;nbsp; Unfortunately, for a couple boards the "BBT" flag was set instead of&amp;nbsp;&lt;SPAN&gt;"BI Swap" (something the manual warns against doing).&amp;nbsp; We tried reprogramming them with the correct settings and while they program OK they do not boot.&amp;nbsp;&amp;nbsp;Tried a full erase, etc., no luck.&amp;nbsp; Any way to recover these boards using&amp;nbsp;ATK or do I need to replace the FLASH part?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 14:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957123#M142989</guid>
      <dc:creator>ambw</dc:creator>
      <dc:date>2019-08-06T14:24:17Z</dc:date>
    </item>
    <item>
      <title>Re: ATK - BI Swap / BBT set incorrectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957124#M142990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Have You&amp;nbsp; tried to erase NAND via the ATK toolkit with BBT option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2019 06:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957124#M142990</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-08-07T06:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: ATK - BI Swap / BBT set incorrectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957125#M142991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I tried that - did not help but one question with erase, what is the proper length value to use with NAND FLASH?&amp;nbsp; It does not seem to be the device capacity (1Gb MT29F1G16ABBHC) as I get "failed:the input operation size exceeds the flash capacity!" with higher values.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2019 14:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957125#M142991</guid>
      <dc:creator>ambw</dc:creator>
      <dc:date>2019-08-07T14:24:13Z</dc:date>
    </item>
    <item>
      <title>Re: ATK - BI Swap / BBT set incorrectly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957126#M142992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please try previous release of the ATK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FSL_ATK_TOOL_STD_1_66&amp;amp;appType=file1&amp;amp;location=null&amp;amp;DOWNLOAD_ID=null"&gt;https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FSL_ATK_TOOL_STD_1_66&amp;amp;appType=file1&amp;amp;location=null&amp;amp;DOWNLOAD_ID=null&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Sep 2019 08:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ATK-BI-Swap-BBT-set-incorrectly/m-p/957126#M142992</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-09-16T08:46:57Z</dc:date>
    </item>
  </channel>
</rss>