<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX Linux compilation problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955180#M142643</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. Does the NXP i.MX series SOC only use yocto to compile and package the kernel, uboot, root file system?&lt;/P&gt;&lt;P&gt;2. Is there a separate BSP patch for Linux, and then add the BSP patch for i.MX to the Linux source code, and then compile it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.请问NXP i.MX系列SOC, 都只能使用yocto编译打包内核, uboot, 根文件系统吗?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.有没有单独提供Linux 的BSP补丁, 然后对Linux源码加上i.MX 的BSP补丁, 再编译的呢?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2019 03:54:37 GMT</pubDate>
    <dc:creator>pengjing918</dc:creator>
    <dc:date>2019-07-23T03:54:37Z</dc:date>
    <item>
      <title>i.MX Linux compilation problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955180#M142643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. Does the NXP i.MX series SOC only use yocto to compile and package the kernel, uboot, root file system?&lt;/P&gt;&lt;P&gt;2. Is there a separate BSP patch for Linux, and then add the BSP patch for i.MX to the Linux source code, and then compile it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.请问NXP i.MX系列SOC, 都只能使用yocto编译打包内核, uboot, 根文件系统吗?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.有没有单独提供Linux 的BSP补丁, 然后对Linux源码加上i.MX 的BSP补丁, 再编译的呢?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 03:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955180#M142643</guid>
      <dc:creator>pengjing918</dc:creator>
      <dc:date>2019-07-23T03:54:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX Linux compilation problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955181#M142644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;1\Yes, the linux BSP use the Yocto.&lt;/P&gt;&lt;P&gt;2\Sorry, no this kind of patch.&lt;/P&gt;&lt;P&gt;I have searched one thread also use Yocto, but Standalone, hope it can do some for you.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-343273"&gt;Detailed Operations For Standalone On Linux BSP of I.MX Processors&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Rita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 05:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955181#M142644</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-07-23T05:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX Linux compilation problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955182#M142645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for your answer.&lt;BR /&gt;Are you an employee of nxp?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 06:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955182#M142645</guid>
      <dc:creator>pengjing918</dc:creator>
      <dc:date>2019-07-23T06:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX Linux compilation problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955183#M142646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome. Yes, many engineers in this community, you can create thread if you have questions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 06:35:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-Linux-compilation-problem/m-p/955183#M142646</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-07-26T06:35:25Z</dc:date>
    </item>
  </channel>
</rss>