<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: What value resistor should pull WDOG_B high?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-value-resistor-should-pull-WDOG-B-high/m-p/955015#M142625</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi adevries&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;100k ohm is sufficient, also one can use internal pull-up as described in&lt;/P&gt;&lt;P&gt;attached i.MX8M Mini EVK schematic p.12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Sep 2019 10:25:45 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-09-21T10:25:45Z</dc:date>
    <item>
      <title>What value resistor should pull WDOG_B high?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-value-resistor-should-pull-WDOG-B-high/m-p/955014#M142624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX 8M Mini hardware developer's guide, table 8, it suggest to pull GPIO1_IO02 (WDOG_B, ball AG13) high with a 100k ohm pull-up resistor. However, in section 5.5 of the same document, Note 2 says to pull the pin high with a 4.7k ohm resistor. Which value is actually recommended?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2019 21:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-value-resistor-should-pull-WDOG-B-high/m-p/955014#M142624</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-09-20T21:55:23Z</dc:date>
    </item>
    <item>
      <title>Re: What value resistor should pull WDOG_B high?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-value-resistor-should-pull-WDOG-B-high/m-p/955015#M142625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi adevries&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;100k ohm is sufficient, also one can use internal pull-up as described in&lt;/P&gt;&lt;P&gt;attached i.MX8M Mini EVK schematic p.12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Sep 2019 10:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-value-resistor-should-pull-WDOG-B-high/m-p/955015#M142625</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-21T10:25:45Z</dc:date>
    </item>
  </channel>
</rss>