<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NXP DDR Test Tool: ERROR: Can't open USB device!!!</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NXP-DDR-Test-Tool-ERROR-Can-t-open-USB-device/m-p/954848#M142590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wonwook&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to attach USB Cable to another connector and&lt;/P&gt;&lt;P&gt;with short quality shielded cable. Also one can check if Operating System&lt;/P&gt;&lt;P&gt;on computer has all latest software updates.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Oct 2019 23:41:42 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-10-08T23:41:42Z</dc:date>
    <item>
      <title>NXP DDR Test Tool: ERROR: Can't open USB device!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-DDR-Test-Tool-ERROR-Can-t-open-USB-device/m-p/954847#M142589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Information&lt;/P&gt;&lt;P&gt;Processor: i.MX6 Solo&lt;/P&gt;&lt;P&gt;Boot Mode: Serial Download ( I checked it several times.)&lt;/P&gt;&lt;P&gt;USB Port: OTG Port&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For SI Test, I once tried DDR Stress test with Ver. 2.8 and it worked fine with my PC.&lt;/P&gt;&lt;P&gt;In Device Manager in Win10, HID and USB Device popped up when USB Cable was connected to my PC.&lt;/P&gt;&lt;P&gt;But, an engineer said that there was the error 'Can't open USB device'.&lt;/P&gt;&lt;P&gt;the engineer checked device manager, but there was no HID or USB Device&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is very weird because I once tried and it worked well but It didn't work to other PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any driver of HID?&lt;/P&gt;&lt;P&gt;or what can I do in this situation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 00:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-DDR-Test-Tool-ERROR-Can-t-open-USB-device/m-p/954847#M142589</guid>
      <dc:creator>wonwookseo</dc:creator>
      <dc:date>2019-10-08T00:50:02Z</dc:date>
    </item>
    <item>
      <title>Re: NXP DDR Test Tool: ERROR: Can't open USB device!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-DDR-Test-Tool-ERROR-Can-t-open-USB-device/m-p/954848#M142590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wonwook&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to attach USB Cable to another connector and&lt;/P&gt;&lt;P&gt;with short quality shielded cable. Also one can check if Operating System&lt;/P&gt;&lt;P&gt;on computer has all latest software updates.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 23:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-DDR-Test-Tool-ERROR-Can-t-open-USB-device/m-p/954848#M142590</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-08T23:41:42Z</dc:date>
    </item>
  </channel>
</rss>