<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to switch EIM control pin to GPIO mode？ in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954752#M142586</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Now I can use EIM and FPGA communication in normal use of imx6sx. the bsp is 4.14.98.CS pin and other control pins are used in EIM.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; As the pins are relatively tight now, I want to switch the CS pins and others used by these EIM to GPIO mode when upgrading FPGA firmware, and then control this pin in the driver. How should we operate to achieve such a function?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I refer to the pinctrl_select_state() function used in sdhci-eshdc-imx..c to switch SDIO pin speed, but an error is reported when I&amp;nbsp;@ using devm_pinctrl_get() to apply for pinctrl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Oct 2019 04:26:03 GMT</pubDate>
    <dc:creator>longh</dc:creator>
    <dc:date>2019-10-23T04:26:03Z</dc:date>
    <item>
      <title>How to switch EIM control pin to GPIO mode？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954752#M142586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Now I can use EIM and FPGA communication in normal use of imx6sx. the bsp is 4.14.98.CS pin and other control pins are used in EIM.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; As the pins are relatively tight now, I want to switch the CS pins and others used by these EIM to GPIO mode when upgrading FPGA firmware, and then control this pin in the driver. How should we operate to achieve such a function?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I refer to the pinctrl_select_state() function used in sdhci-eshdc-imx..c to switch SDIO pin speed, but an error is reported when I&amp;nbsp;@ using devm_pinctrl_get() to apply for pinctrl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 04:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954752#M142586</guid>
      <dc:creator>longh</dc:creator>
      <dc:date>2019-10-23T04:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to switch EIM control pin to GPIO mode？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954753#M142587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi long&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to write to iomux registers directly, use as example memtool:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=imx_4.14.98_2.0.0_ga"&gt;memtool\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 10:22:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954753#M142587</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-23T10:22:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to switch EIM control pin to GPIO mode？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954754#M142588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much！&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; I will try this way. Can Linux API achieve the same function?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2019 03:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-switch-EIM-control-pin-to-GPIO-mode/m-p/954754#M142588</guid>
      <dc:creator>longh</dc:creator>
      <dc:date>2019-10-25T03:56:22Z</dc:date>
    </item>
  </channel>
</rss>